Part Number: TAS5720M Hello,
I'm working on a project using the TAS5720M. I've created a small breakout board for the amplifier (24 V) and am working on running some basic I2S audio with an ESP32-S3-N8-R2.
I've had success reading I2C registers, but…
Part Number: TAS5720M Tool/software: I am trying to generate a tone on an 8-ohm speaker using ESP32 with I2S. Working conditions:
SAIF: I²S
16-Bit Data, I2S_SLOT_BIT_WIDTH_32BIT
RCLK = 48 kHz
BCLK = 3.072 MHz
MCLK = BCLK
But I was not…
Part Number: TAS5825M Other Parts Discussed in Thread: TAS5720M , TAS5805 Hi Expert,
My customer have design and want to use TAS5825M to drive Tweeter and use TAS5720M to drive Woofer.
For Woofer will need 5W*2 and Tweeter need 3W*2.
May I know…
Part Number: TAS5825M Other Parts Discussed in Thread: TAS5720M We are developing a 2.1ch system with TAS5825M and TAS5720M.
In PPC3, I set up the AGL woofer as shown in the picture below and developed it by downloading the [dump to header file].
…
Part Number: TAS5720M Other Parts Discussed in Thread: TAS5805M , TAS5825M , TPA3111D1 , TPA3116D2 , TPA3118D2 Hi Team,
May I have PSpice module of TAS5720M? I can't find it in PSpice software, or even TAS5720M website, I need it to do simulation…
Part Number: TAS5720M Hi,
on TAS5720M datasheet package outline and footprint are missing. Can you provide dimensions and recommended footprint?
Best regards, Marco
Part Number: TAS5720M Hi,
Please refer to the question my customer is having below:
The AIC3254 GUI command window cannot currently change TAS5720m register, screen shot shown as below:
Please let us know if there are further information…
Part Number: TAS5720M I am trying to get the tas5720m to initiate in linux (kernel version 4.14). But there are problems initializing the pvdd:
tas5720@6c {
compatible = "ti,tas5720";
reg = <0x6c>;
pvdd-supply = <®_pvdd>;
dvdd-supply = <®_dvdd…
Part Number: TAS5720M The datasheet of the TAS5720M shows an application circuit which does not include an LC filter on the output.
The EVM for the TAS5720M does implement a LC filter on the output.
Thee is no discussion in the datasheet or EVN user…