Part Number: TAS5721 Other Parts Discussed in Thread: TAS5720M I'm looking to use the TAS5721 as a mono amplifier, but I don't need the additional power that PBTL provides, and would rather not spend the money on the additional output filter components…
Hi Jon,
TIDA-060026 (TAS5825EVM-SB) is scalable to 5.1, 7.1 and 9.1 channel configurations, and it's just used to show 2.1 configuration demo.
As for the capability of multiple channel audio interface with PPCMB, it could use PSIA input with TDM modes…
Hi Jared,
Actually our closed-loop class-d products are being widely used in the ultra-sound apllication. It can support upto 75kHz loop bandwidth, but you need to redesign the LC output filter. Do you have TAS5720M EVM board? You can do filter tuning…
Part Number: TAS5720A-Q1 Other Parts Discussed in Thread: TAS5720L , TAS5720M
Hello community,
we currently have some issues with the TAS5720A-Q1. According to the datasheet, I²C should be active after 12 ms. In our case we power the TAS5720A-Q1 for…
Hi Shawn,
I have the following EVMs:
TAS5720M
TAS5760XX
TAS5766MDCA
PUREPATH-CMB
PP-SALB
I have been granted access to the PPC3 App and have downloaded and installed. But the only EVM App that is available is the I2C Master
My account is…
Hi Dan,
Apologies for delayed reply.
Here we want to add redundancy in the system . So we are feeding the output of Power Amplifier from two different systems which are rated to Drive 8Ohm 25W speakers. In our system we will feed this signal to an…
Hi, Wayne,
Unfortunately, we don't have a specific GUI for the control of the TAS5720MEVM. This device doesn't have many configuration options so the use of a general I²C tool (like the I²C monitor in PPC3) can be used to program the TAS5720M.
Best…
Hi Kamal, The TAS5720L is a good comparison device for this product. Depending on their available power supply, the TAS5720M is also a good selection as well, because it can do higher power than what the Maxim part can do.
Please feel free to have…