Part Number: TAS5727 Other Parts Discussed in Thread: TAS5538 , TAS5352 , Our customer has done the HD DTS certification test, but has failed. While another one TAS5538+TAS5352 has passed.
In the test, the signal source will output 3 kind of signals in different…
Other Parts Discussed in Thread: TAS5727 I am debugging a board I designed using the TAS5727 in mono PBTL mode, using 16-bit I2S with an LRCK of 48kHz (Fs), SCLK of 1.536MHz (32Fs), and MCLK of 12.288MHz (256Fs),
I currently have it set up as follows:
…
Part Number: TAS5727 Whenever the "exit shutdown" command is sent (value of 0x40 to register 0x05) in preparation for normal operation, the TAS5727 plays a high-pitched whistle that lasts exactly the time specified by register 0x1A. Once the whistle stops…
Other Parts Discussed in Thread: TAS5727 Hi,
I'm using a TAS5727 digital audio power amplifier and have some questions about initialization. Presently, I have the RESET pin being held HIGH shortly after my unit (the product being worked on) powers up,…
Other Parts Discussed in Thread: TAS5727 Hi,
We are using two TAS5727 digital amps in a product, and we are observing that one of the amps (the same one each time and only that one) sporadically shuts down. When this happens, many register values change…
Other Parts Discussed in Thread: TAS5727 Hi,
Using the TAS5727 in a product, we are seeing current limit occurring at about 3A, whereas the amplifier spec says over-current limit protection is 4.5A nominal. Do you have any insight about this discrepancy…
Other Parts Discussed in Thread: TAS5727 , TAS5751M Hi Team
I want use TAS5727, My speaker impedance is 4 ohm +/- 15% , The load Minimum will be 3.4 ohm.
TAS5727 spec show the load Minimum is 4 ohm.
Could we use TAS5727 in our system? Did you have any…
Other Parts Discussed in Thread: TAS5727 I'm trying to use the TAS5727 GDE to adjust the DRC parameters, but the UI I see on the computer screen is completely different than the description in Application Report SLOA148-June2010. The GDE software version…