Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: TAS5727 Hi...
My customer wants to configure the BTLx2 Output Stage (@ 4ohm, THD+N=10%) of TAS5727.
But I could not find the graph data of output power vs supply voltage in datasheet.
So I need the graph data as follows…
I am also working on a design using the TAS5727, 18V PVDD. I am only looking to drive 20W out to one channel, but I am very space constrained and am also looking for a smaller alternative to the TOKO inductors.
Did you find something you could recommend…
Other Parts Discussed in Thread: TAS5727 Hi
I am having problems getting audio from TAS5727.
SDin = audio data
LRclock = 44.1 KHZ
Sclk = 2.1 Mhz
Sclk linked to Mclk
I send over I2c
0x1B,0x00 Trim
0x00,0x60 Control 1, 44.1/48-kHz sample rate, MCLK frequency…
Other Parts Discussed in Thread: TAS5727 Dear TI community,
I need some clarification regarding the oversampling in TAS5727 audio amplifier. We want to use TAS5727 for our module which can generate only 16 bits of data per channel but we want to be in…
Other Parts Discussed in Thread: TAS5727 , TAS5727EVM We’re working on a project that uses a Bluegiga WT32 Bluetooth module as an A2DP SINK and sends the audio data out of the WT32’s I2S interface to a TI TAS5727 amplifier chip. To assist with development…
Dear Sir
we use i2c memory tool read address 0x00 data is 00. but Initialization data should be 0x6c.
Is my operation some thing wrong?
Best regards,
Bogey
Other Parts Discussed in Thread: TAS5727 Hi,
currently we are using TAS5727 amplifier in our design.
Presently we have connected MCLK input to oscillator.
Is it ok ?Do we need to connect MCLK to SCLK?
which is the best option?
Other Parts Discussed in Thread: TAS5727 , TAS5760MD , TAS5760M , TAS5708 Hi,
When looking through the datasheet of the TAS5727 I could not find the PSRR. I would like to know the PSRR of the TAS5727, because I am contemplating if I need to make a clean…
Other Parts Discussed in Thread: TAS5727
Normal
0
false
false
false
MicrosoftInternetExplorer4
Hi
I am currently developing a circuit board using TAS5727. But I can not get any audio output.
The I2S Da…
Other Parts Discussed in Thread: TAS5727 Hi,
Is there anyway I could obtain just the small eval module for the TAS5727 as I already own the MC57xxPSIA board (from another evaluation kit we bought)
Thanks