Hi, Sean,
I performed some tests in the EVM. I have no issues with the TAS5715 GUI, but after opening the GUI I noticed that the default process flow on the GUI is the TAS2727. After connecting the TAS5715 with the TAS5727 GUI, I was able to replicate…
Other Parts Discussed in Thread: TAS5717 , TAS5707 , TAS5727 Hi,
What kind of concern point is there if replacing TAS5707 with TAS5717 ? Could you please give us your advice about it ?
Best regards, Kato
Hi Ben,
The datasheet specifies the usage of 0.1µF capacitors to decouple the high frequency components of the power supply, these should be placed as close as possible of the Amplifier. The TAS5727 requires also big bulk capacitors to remove low…
Other Parts Discussed in Thread: TAS5727 , TAS5707 Hello
Thank you for your daily support..
I have theree questions about TAS5727 data sheet, Please give me your advice.
My client intends to use TAS5727 with PBTL 40W.
Q1 My Client want to use big ( 1500uF…
Other Parts Discussed in Thread: TAS5727 , CC8520 Hello,
in Wireless newsletter, in PurePath Wireless section, near the Wireless Headset/Headphone refernce design it is refered a reference design "Wireless speakers 25W Class-D". (CC8520+TAS5727+LM2842Y…
Hello Max,
Almost all TAS57xx devices can be implemented in PBTL. In the case of TAS5717/19, effectively the wiring between the outputs should be done after the LC filter. Newer devices like TAS5727 supports single filter PBTL mode.
You need to take care…
Other Parts Discussed in Thread: TAS5711 , TAS5727 , TAS5731M
Hello
My client intends to use TAS5711 as single filter PBTL like attached schematic..
However, there are big POP when PWM had ON ( 0x05= 00) ( wave form attached.
blue and light-blue is each…
Other Parts Discussed in Thread: TAS5727 Hello,
I would like to have help.
(1)
I am using TAS57xx GDE. After finish the EQ ,DRC and so on,
I want to save all of setting as .cfg file into PC, But I have no idea about how to generate the cfg file and save…
Hi, Srinivas,
cc8520 transmits i2s data. So, you need something that can handle an i2s data source at the other end (either anothr PCM3070 or a TAS5727 for example).
We have a separate e2e for the cc8xxx devices. I suggest you post questions specific…