Part Number: TAS5731M Hi Team,
What is the function of register 0x10 of tas5731m? Why is the modulation limit must be set to 93.8% when the supply voltage is greater than 18V?
Thanks and regards
Part Number: TAS5731M Hi,
In the design, the MCLK is not used. So, how the MCLK pin is connected?
Can it be connected to the ground or floating?
Can it be connected to the Capacitance to ground as shown in the picture?
Thank you so much!
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5731 Dear TI team
I'm going to learn two questions from you about TAS5731M
Whether 4th Order LinkWitz-Riley is supported in TAS5731M EQ Settings , whether support or not Multiorder…
Part Number: TAS5731M Hi team
Customer conducted the test that whether TAS5731M can recover form the High PVDD voltage. they set the PVDD to 27.5V which not exceeds the maximum value in datasheet, but after 2mins, the device cannot generates the output…
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5731 , TAS5805 , TAS5805M Hi,
I have some EQ in TAS5731M which has positive gain (10dB) at a particular frequency.
What the maximum gain a 0dB input signal can have (without digital clipping…
Part Number: TAS5731M Hi team.
In the EVM user guide of TAS5731M, I see the bootstrap cap is 0.0033uF. If it's OK to use 0.022uF、50V, X7R? How can you evaluate the capacitance is proper?
thanks a lot.
Best regards,
Yang
Part Number: TAS5731M Hi Team,
There will be no sound after -15 degrees of power on, and normal after restart.
According to the log, the customer found that the osc_trim register value was abnormal, sometimes 82, sometimes 00. But the correct value…
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5760M , Dear Sir,
What is the signal latency (or processing time) from I2S input to Class-D output for TAS5731M and TAS5760M, with EQ and DRC enabled?
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5731 Hi TI experts,
Is it possible to provide HTOL data for the reliability data of TAS5731?
It can usually download reliability data from ti.com, but for TAS5731, HTOL is not listed.
TAS5731MPHP…