Part Number: TAS5753MD Hi,
I have two questions related to bringing up a TAS5753MD board.
1) The TAS5753MD is responding to 7bit i2c address 0x2B (for example, I read back the correct device id from reg 1) confirmed with logic analyzer, and it is the…
Part Number: TAS5753MD Hello TI Team, we are working on a new project with the TAS5753MD. Actually, we've got troubles to get some sound of it.. We ensured that the Start-Up and Power-Down sequences work properly - as mentioned in the datasheet. The result…
Part Number: TAS5753MD I just got my TAS5753MD dev board, and need to connect the power terminals. Spec says that any input voltage from 8V - 26V will work. But I so not want to damage the board, and I was also curious, can the PVDD be 5 Volts?
Part Number: TAS5753MD
Hi Team, Customer uses TAS5753 line out driver. If customer would like to implement 2rd butter-worth low pass 22kHz and gain 2V/V circuit, do we have recommended tool for this?
BR, SHH
Part Number: TAS5753MD The TAS5753MD datasheet suggests that the default device ID (register 0x01) is 0x41. I'm reading 0x3D. Is there any significance to this number?
Part Number: TAS5753MD Hi Dear TI members,
Recently, i am studying the TAS5753, but i found the register table is not complete(eg. i just found the 0x18 is missing, and from the datasheet description, the section 8.5 is missing too), so may i know how…
Part Number: TAS5753MD
Hi Team,
customer has question for some register and some reserved registers.
could you please provide your comment on the register byte definition?
(1) subaddress 0x3A BYTES NUMBER and datasheet DEFAULT VALUE byte number are…
Part Number: TAS5753MD
Dear E2E member,
Could you confirm the questions as below?
1. Please refer the picture as below, When PVDD=24V, use Stereo BTL mode, the IC can drive 2 speaker of 15W(4Ω). Is it correct?
2. Please refer the picture as below…