Hi Jesse-san,
The AP which I mentioned above is an abbreviation for "Auido Precision". I understood that a sound doesn't come out if applying I2S signal to TAS5754MDCAEVM via BT module which you used. So, does TAS5754M work normally if using…
Part Number: TAS5754M I wanted to verify the output power of a Texas Instrument class D EVM (TAS5754MDCAEVM) After hooking up a 4 ohm test load and a 24V 5A power supply I got the following waveform after the LC output filter (see attachment) If I reduce…
Hi Wayne,
Yes, HybridFlow 2 of TAS5754 supports 2.1CH output. Two devices are needed for that application (which is what TAS5754MDCAEVM does).
Please refer to page 12 of the attached document for more detail. slau577a.pdf
Thank you!
Best regards,
-Roy H…
Hi Kenneth,
Below is the PCB file of the TAS5754MDCAEVM that shows all the 4 layers. I think it should be what you are looking for now.
TAS5754MDCAEVM PCB.pdf
Andy
Other Parts Discussed in Thread: TAS5754MDCAEVM Hello,
I requested this development software on Monday morning. I have not received any kind of feedback. Is there any way to get a status on this request? I have a PPCMB + TAS5754MDCAEVM and I want to bring…
Hi Rick,
Usually the PPC2 is the tool we use to write the correct FWID for each TAS5754MDCAEVM. Unfortunately, that tool is not able to work in your case.
Did you write the FWID to "FWIDTAS5760CCEVM-A" in PurePath Console 1? Can you try again so…
Hi Kato-san,
You don't have to remove any components from the PurePath CMB and the EEPROM will not affect the configurations.
Below are the steps.
Step 1: Connect a micro USB cable to PurePath CMB and PC.
Step 2: Connect a power supply to TAS5754MDCAEVM…
Part Number: TAS5754M hi
1. I setup TAS5754MDCAEVM with PurePath Console2 GUI.
2. Tie the MCLK(Pin 22) to GND or Connect MCLK(Pin 22) directly to SCLK(Pin 23)
3. And then set the Registers value as below, which is found in E2E forum
There is no audio output…
Hi, Kato-san,
In the EVM Product Folder for TAS5754M, there is a link to request access to the GUI in the Description field:
Description
The TAS5754MDCAEVM allows evaluation of the TAS5754M I2S-input, closed-loop amplifier. It is populated with two TAS5754MDCA…