Part Number: TAS5755M Dear TI Support Team,
I am currently evaluating the TAS5755M Evaluation Module for an audio amplifier design project.
I would like to request the following files for the TAS5755M EVM, if available:
Gerber files
Any additional…
Part Number: TAS5755MTAS5755M output PWM wave is ok, but no sound output. Could you provide I2C code? The input I2S signal is connected to the DAC, and the output sound is no problem.
Part Number: TAS5755M Dear TI group,
We use TAS5755M drive a Subwoofer with 3R@40W, and OUTPUT power=32W,Appendix show config and Schematic,
after work on a fewer miniute,TAS5755M occurs a error output state,OUTA&B=14V ,OUTC&D=0.4V。
What are the…
Part Number: TAS5755M TAS5755 i n the PBTL mode, only B and D channels have output, but A and C channels have no output, and there was no VCC/2 level. This is very different from the specification. What is the reason for this problem? There is no problem…
Part Number: TAS5755M Hi Ti Team,
When TAS5755 is in Mono 1.1, it is found that the DRC of the treble and the bass cannot be completely separated; the DRC can be well controlled when the treble is input only or the bass is input separately. There will…
Part Number: TAS5755M I'm using a TAS5755M in an application. I have it mostly working as required (2.1, BD mode, biquads used as active crossovers and bass/treble shelf filters). I'm trying to get DRC working but am finding a dearth of documentation…
Part Number: TAS5755M I have a TAS5755M configured in 2.1 BD mode. The center (BTL) channel is fine but the two SE channels pop loudly when started up after a cold boot. The weird thing is that they don't pop anywhere near as loud when restarted after…