Part Number: TAS5755M TAS5755 in 2.1 mode: When choosing 2.1 mode,How many watts can the maximum power be achieved?
working voltage:12v
TAS5755 in 2.1 mode: Can the following three audio output power be achieved? (speakers:12W,4Ω) 1 Group: 12W Audio…
Part Number: TAS5755M TAS5755 in 2.1 mode: When choosing 2.1 mode,How many watts can the maximum power be achieved?
TAS5755 in 2.1 mode: Can the following three audio output power be achieved? (speakers:12W,4Ω) 1 Group: 12W Audio Output (full frequency…
Part Number: TAS5755M Hi,
TAS5755M have some setting question in my product.
1, on the speaker sound power, the motherboard side is -12db, 1Khz is 8W, But 0db will exceed 10W, how to adjust? 2, subwoofer problem: (1) The customer asks bass to disable…
Part Number: TAS5755M Other Parts Discussed in Thread: TAS5731
Hi Team, My customer uses TAS5755 and tune by TAS5731 GUI. Customer has question why the same DRC setting on TAS570x1 and PPC1.16 has different result input/output chart. Could you please let…
Part Number: TAS5755M Other Parts Discussed in Thread: TAS5751M
Hello
My customer had bought / evaluated TAS5755M EVM with 2.1ch configulation.
The reason why TAS5755M chosen is price.
The application is sound bar ( 20W x 4 + 40W x2) , so we thought…
Part Number: TAS5755M
Hi Team, Cusotmer has two question for the TAS5755.
1. What is the Peak and RMS meaning in the DRC setting? I saw the dump register has difference on the 0x3B/0x3C/0x40.
2. What is the signal flow for the PBTL in the GUI? and how…
Part Number: TAS5755M
Hello
My customer intend to use 2.1ch for TAS5755M .
I had tested TAS5755MEVM by myself.
SSTIMER pin is as default ( 2.2nF is between SS timer and gnd)
In case 0x1A register is 1Ah ( SSTIMER enabled), POP is seen, 0x1A is 88h, no…
Part Number: TAS5755M Hi Sirs, Would you please advise the TAS5755's maximum PBTL output power with 3ohm load, 24V PVCC? Customer found the TAS5755 can be damaged with >70W PBTL, 3ohm load. Can this device achieve 100W in PBTL mode? Thank you and Best…
Part Number: TAS5755M The TAS5755MEVM.pdf document shows the diagram below where the non-driven side of a single ended (SE) output has SINGLE-ENDED SPLIT-CAPs and/or do-not-populate resistors in a potential divider. This is confusing because the data…
Hi Menaka,
My response below:
1. Din should be connected to SDIN, not an output.
2. A host processor is still necessary for communication with the CODEC.
The TLV320AIC3204 does not have any internal class-D amplifiers so you would not be able to achieve…