Part Number: TAS5760LD Hi Team,
Please help me answer the follow question, thank you so much.
Jitter is occurred in the “I2S_SCLK”. It was found that noise is generated in the audio signal due to this jitter. Is there a setting that can reduce the effect…
Part Number: TAS5760LD
Hi team,
customer has some speaker damage issues, do you knowhow to set DCE threshold? from register 0x08 bit 1, it only show DCE event.
from d/s table 2, it showed the DCE will be triggered at 2.6V at PVDD 12V conditions.
BR, S…
Part Number: TAS5760LD
Hi team, customer uses TAS5760*2 and TAS5753 for stereo, two woofer and center application. Do you have idea how to use AP or other tool to generate the 4.1 CH source for customer test?
BR, SHH
Part Number: TAS5760LD Hi, I was just wondering what type of DAC is used in this chip (TAS5760).to convert the I2S data sample to PWM samples. Does it have a particular name?
-Erblin
Part Number: TAS5760LD Other Parts Discussed in Thread: TAS5760L Hi
For our project we do not need the headphone output. Can the DR_INA/DR_INB, DR_OUTA/DR_OUTB, DR_MUTE, DR_UVE, DR_NC and DR_CP be left unconnected? We are using the Mono PBTL Using Software…
Hi Ravi,
I intend to use the digital clip level function in the TAS5760LD.
However, I am confronted with a kind of attack/decay behavior which is detoriating the audio performance substantially.
With a sinewave, it is working fine. But with music you…
Other Parts Discussed in Thread: TAS5760LD , TAS5760MD , TAS5760L Hi folks,
In TAS5760LD datasheet, there are two THD+N vs Output Power graph in the same condition.
For example Figure 5 and Figure 6 in page 14, as below picture:
What's the difference…