Part Number: TAS5760M Hi team
I have a question about power consumption.
The conditions of use are as follows.
【conditions】 PVDD: 24V Rspk: 8Ω SPEAKER AMPLIFIER STATE: fspk_AMP =768kHz,Shutdown
【question】 ①The following values listed in the…
Part Number: TAS5760M Dear teams,
There is an issue that our LSI cannot get ACK from the device when accessing registers via the I2C control port.
This phenomenon is occurring on our multiple test boards.
When accessing the I2C control port, we…
Part Number: TAS5760M
Team, Can we please help with the belwo question:
We use the amplifier in BTL (stereo) mode (In case needed I can share the TAS5760 portion of the schematic off-line if needed). However we now need to drive a speaker with less…
Part Number: TAS5760M-Q1 Tool/software: Hi, Team
I know when TAS5760 set to hardware mode, SPK_SLEEP/ADR is used for SLEEP function, and if the TAS5760 set to software mode, users can use SPK_SLEEP/ADR pin to set the i2c address.
But my customer prefer…
Part Number: TAS5760M-Q1 Tool/software: Hello,
I am working on TAS5760M-Q1.
At the power up, I set the following registers :
REG ADDRESS
DATA
0x02
0x04
0x01
0xFD
0x06
0x51
The others are kept as default…
Part Number: TAS5760M-Q1 Hi TI team,
We have requirement for class D audio amplifier for automotive application.
It should driver x2 5W, 8 ohm speakers.
Audio type Stereo.
Also, it should support load diagnostics
TAS5760MTDAPQ1 , meets above…
Part Number: TAS5760M-Q1 Hi E2E,
As the datasheet of TAS5760M-Q1 shows that : Supply Voltage at 14V 、RL= 4 Ω、 THD+N 10% . The max output power=25W.
I want to know i f we design an application on this condition( Supply Voltage at 14V 、RL= 4 Ω、 THD…
Part Number: TAS5760M Hi team,
I have a question about output noise.
The noise after the output stops is different each time.
When there is no output after the power is turned on, it is almost the same every time, but after outputting, the noise…
Part Number: TAS5760M Hi.
The output of the amplifier appears smaller than the calculated value. Also, I checked the output of several amplifiers, but the output varies.
The following setting values:
・Serial Audio In: -6dB sine wave (1kHz) ・Digital…