Part Number: TAS5766M
Tool/software:
Hello,
I am working on a project where I would be using the TAS5766M and another I2S IC in TDM mode since my processor only has 1 I2S interface. The data sheet for TAS5766M states that you can enable one of the…
Part Number: TAS5766M Hi Team,
Customer would like to design TAS5766M at PVDD 20V case.
Would you please help review and provide your comments on the current in 20V case?
d/s only indicate 12V and 24V case.
Thanks for help!
SHH
Part Number: TAS5766M I have two speakers in my design. I would like to drive two speakers in mono mode with TAS5766M. Only one of the speaker requires smart amp. The second speaker does not require smart amp mode and can be driven in basic mode. Is it…
Part Number: TAS5766M
Greetings
on a custom board we are trying to bring up TAS5766M part.
we are feeding BCLK, LRCLK and I2S data to I2S input port and can see same audio appear on I2S output (SDOUT). However there is no signal present on DACR…
Part Number: TAS5766M Tas5766 has some problems, please help solve them. 1. Under normal conditions, when EQ is not added, DC15V is used to supply 4 ohm load, and the maximum output of horn end is about 9V, which begins to be distorted.
2. When EQ…
Part Number: TAS5766M Hi Team,
1. Is there a low power mode or sleep mode for this IC? How is it achieved?
2. Regarding XSMT, if I use the mute function of the audio codec, do I still need to set the XSMT mute function? Best Regards, Jaden Yue
Part Number: TAS5766M Hi team,
Customer comes to us to check about the TAS5766 learning board schematic. The learning board on their hand is as follow, I can't find the board and related materials, could you help check if we still get the schematic…
Part Number: TAS5766M We are using the TAS5766M in a Mono configuration where the OUTPR/OUTNP (OUT_RIGHT) are tied to one speaker terminal and the OUTPL/OUTNL (OUT_LEFT) are tied to the other speaker terminal. The TAS5766 is powered by +12V DC for the…
Part Number: TAS5766M Hello,
Need help with TAS5766M implementation for custom board we are developing. The target application is 8 ohms 5W continuous and 8W peak power speaker. PVCC is 24V.
The issue is following Audio mutes for 1.3s when there is…
Part Number: TAS5825M Other Parts Discussed in Thread: TAS5766M Dear Audio support team,
This is FAE Dave located in Taiwan.
Due to the supply issue, our customer wants to co-layout TAS5825 with TAS5766M(VQFN package).
Since they have the limited…