Part Number: TAS5766M We are using the TAS5766M in a Mono configuration where the OUTPR/OUTNP (OUT_RIGHT) are tied to one speaker terminal and the OUTPL/OUTNL (OUT_LEFT) are tied to the other speaker terminal. The TAS5766 is powered by +12V DC for the…
Part Number: TAS5766M Other Parts Discussed in Thread: TAS5768M , Volume block, from -110 db to +6 dB with 0.5 dB steps, including a fixed gain block of 0dB to 12 dB gain.
this mean is ?
i have linux drive about 5766m (Linux Driver for TAS5766M and TAS5768M…
Part Number: TAS5766M Hi,
for TAS5766M, I implemented Ra and Rb so that the PWM frequency is 768kHz, but the actual output PWM frequency is 384kHz.
Two of the six prototypes have this symptom.
What are the possible mistakes?
Part Number: TAS5766MRMTEVM Other Parts Discussed in Thread: TAS5766M Hi TI experts,
TAS5825 and TAS2805 were able to apply for APP on TI web. however, the TAS5766 cannot find the APP on the TI web.
Could you provide TAS5766M APP in purepath3?
This is…
Part Number: TAS5766M Hello,
Need help with TAS5766M implementation for custom board we are developing. The target application is 8 ohms 5W continuous and 8W peak power speaker. PVCC is 24V.
The issue is following Audio mutes for 1.3s when there is…
Part Number: TAS5766M Hi Sirs, Would you pls advise the full scale output of the TAS5766 and TAS5825's SDOUT of Post Processing? My customer would like to know the relationship between Class-D's Vout vs SDOT's dBFS of the TAS5766 and TAS5825.…
Part Number: TAS5766M Hi team,
My customer is using TAS5766M in their speaker application and recently encounter an issue of no output when performing a AC off/on while the video and audio still streaming.
Their analysis suspect that the decoded I2S audio…
Part Number: TAS5766M Hi team,
Hope you're doing well! My customer has an urgent issue regarding this chip. They are hearing a "popping" noise coming from the smart amp. They've received returns from multiple different ECs across multiple units. Please…
Part Number: TAS5766M Team,
Customer is using learning board to characterize a speaker using speaker model "single driver passive radiator". However, customer now is not able to drill the hole to the speaker cabinet. Looks like this step can not be skipped…