Part Number: TAS5766MRMTEVM Other Parts Discussed in Thread: TAS5766M Hi TI experts,
TAS5825 and TAS2805 were able to apply for APP on TI web. however, the TAS5766 cannot find the APP on the TI web.
Could you provide TAS5766M APP in purepath3?
This…
Part Number: TAS5766M Dear Sirs,
My customer uses TAS5766MEVM.
Then they started up PPC 3 and checked the operation. Next, after system calibration, clicking on the tuning screen will freeze on the display of "Updating Components". So I also confirmed…
Part Number: TAS5766M Hi team,
My customer is using TAS5766M in their speaker application and recently encounter an issue of no output when performing a AC off/on while the video and audio still streaming.
Their analysis suspect that the decoded I2S…
What you you mean by 1.1 PBTL mode? Do you mean you want to use two TAS5766M devices and each of them works in PBTL mode?
We have only designed a stereo(2.0) SmartAmp flow for TAS5766M. If you are designing a 1.1 system using just one TAS5766M device…
Part Number: TAS5766M Hi Sirs, Would you pls manage TAS5766M efficiency with 4ohm load, 17V PVCC condition? Before the actual number, can I assume the TAS5766M's efficiency around 70% (between 12V and 24V's curve) with 2W, 4ohm load? Thank you and Best…
Part Number: TAS5766M Hi Sirs, Would you pls advise the full scale output of the TAS5766 and TAS5825's SDOUT of Post Processing? My customer would like to know the relationship between Class-D's Vout vs SDOT's dBFS of the TAS5766 and TAS5825. Thank you…
Part Number: TAS5766M TAS5766 PP3 CAN NOT USING THE Interface ----why,using win7 &win 10 or so can not using the timing,but can connect the TAS5766EVM master interface
the always show “updating components”
Part Number: TAS5766M Hi team,
My customer is evaluating the TAS5766M now. We meet some problems about TAS5766M.
Few questions want to check with you.
1. Can the chip support 4k sample rate(LRCK = 4kHz)? 16Mhz SCLK to BCLK128k to 4k LRCK, BLCK/LRCK…