Part Number: TAS5805M Hi,
Plesae advise if TAS5805M can support the 10W output power because our loudspeaker is 10W max., and now, there are much burst sound on high volume but there are no brust low volume;
We use the BTL mode, and the AMPLIFIER PEAK OUTPUT…
Hi Yunchuan
The 29.5 is TAS5805M's default Gain, the amplifier's Gain is not related with PVDD voltage. We should start calculation with the default Gain value.
Of course with 12V supply, the output will clipped at 12V. But a clipped at 12V w…
Part Number: TAS5805M Could you please clarify the following points regarding the DSP_MISC control register?
What is the function of bit position 3? The description "Left and Right will have use unique coef 0->Right channel will share left channel coefficient…
Part Number: TAS5805M Hello,
Regarding to the GLOBAL_FAULT1 on TAS5805M, my customer is asking a question.
What kind of errors are OTP_CRC_ERROR and BQ_WR_ERROR in register "GLOBAL_FAULT1"?
What do "OTP" and "BQ" mean?
…
Part Number: TAS5805M Other Parts Discussed in Thread: TAS5805 Hi team,
Customer get one question about the following LC filter recommendation in TAS5805 datasheet.
Their input voltage is 15V, and use 1SPW mode, based on the table, we recommend 15uH +…
Part Number: TAS5805M
Hi. We have a problem with TAS5805M. There is no sound. The sound source is a Bluetooth module via I2S. We have tried the following
The bluetooth module is set to 44.1KHz 16bit.
The following registers are set, rest is default…
Part Number: TAS5805MEVM Hi,
Do you know the frequency response of this evaluation board? For example I can manage to send a sine wave at 15 kHz but from 20, 22 and 25 kHz on the signal is heavily attenuated. Is there an additional output filter different…
Part Number: TAS5805M Hi team,
Customer design speaker amp with below condition
Load 4ohm
THD+N 10%
Output power 15W
Can TAS5805M achieve this performance?
Is this graph being indicating "maximum output power"?
Best regards,
Hayashi
Part Number: TAS5805M Hi Team,
Could you please share how to set the 4000Hz crossover point to output treble/bass audio from the left and right channels respectively. How to implement it on TAS5805EVM? Does it require hardware circuit adjustment? How to…