Part Number: TAS5806M Other Parts Discussed in Thread: TAS5805M , , Hi TI experts,
Customer line has been down because of lead time issue of TAS5805M. So it needs to be replaced with another solution.
I confirmed that the register map of TAS5806M is the…
Part Number: TAS5806M Hi TI experts,
We are using the TAS5806MEVM to test the DRC control.
Set DRC as below.
We are measuring the frequency response. however, this is different from the PPC3 graph. There was a gain at 250Hz and 15kHz.
See the Cyan color…
Part Number: TAS5806M Hi TI experts,
Regardless of the input level, We want to set the 80 Hz band to the same output.
The attached file has the graph we want and the TAS5806M output graph. Please check the attached file.
Request.xlsx
We tried to attach…
Part Number: TAS5806M Hi everyone I have created an a2dp project using an esp32 and the TAS5806M. The bluetooth audio is fine and I have no problems. Now I am trying to integrate the HFP profile to be able to make hands-free calls. I set the sample rate…
Part Number: TAS5806MD Other Parts Discussed in Thread: TAS5806M TI does not have enough stock of TAS5806M chips, and offered TAS5806MD instead. The difference between the two chips is that TAS5806MD option has a headphone amplifier. I do not need it…
Part Number: TAS5806M Other Parts Discussed in Thread: TAS5805 Hello everyone. I tested the TAS5806M powered at 12V and everything works perfectly, but if it is powered at 24V the TAS5806M heats up and immediately goes into protection. What am I doing…
Part Number: TAS5806M Other Parts Discussed in Thread: TAS5805M , I have a design based on the TAS5806M.
I'm running it from PVDD=+24V, DVDD=+3.3V
However I'm seeing the audio output voltage (+ and - output) sitting at ~5V when the output is idle…
Part Number: TAS5806M Hi,
I am testing my TAS5806M design. The design works fine with a 4ohm speaker.
I would like to test system power draw by substituting a 4ohm power resistor for the speaker. So - I have a 4ohm 5W resistor load connected to one of…
Part Number: TAS5806M Team,
Do we have any tool or equation to calculate the power dissipation for TAS5806M at the given condition? For example, input voltage, audio output power, speaker ohm, etc.
Thanks,
Best regards,
Andy Chu