Hi Severin
About the noise in pvdd, have you check your GND of power supply, is it been connected together with amp gnd.
is there any place where GND hasn't been connected together.
noise in bclk, i think it should be ok if amp can play the sound…
Part Number: TAS5806MD Hi, TI suppor team
Is it possible to control the headphone volume of the TAS5806MD product through the remote control of the finished product?
Thanks.
Regards,
MJ
Part Number: TAS5806MD Has anybody measured the output latency of TAS5806MD device?
I would like to use the TAS5806MD, over a solid state Class D amp, as it simplifies my design massively, without adding too much extra cost and bringing a whole load of…
Part Number: TAS5806MD Other Parts Discussed in Thread: TAS5806M Hi, TI Support Team
A customer is reviewing TAS5806M and TAS5806MD in parallel.
Is it okay if I connect the H/P pin shown in the picture below to GND?
Thanks.
Regards,
MJ
Part Number: TAS5806MD Hi, TI support team
A customer is reviewing the TAS5806MDEVM and its actual application.
I am trying to test by turning on DRC, but please let me know which part of the register setting should be done.
If it is in the datasheet…
Hi MJ.
Sorry for replying you late.
MJ Jeon said: Is the product capable of DRC and Tone Control?
Yes, TAS5806 has the functions you mentioned, you can configure it through by PPC3 software.
Meanwhile you can take below material as a reference.
TAS5805M…
Part Number: TAS5806MD We have SCLK, LRCLK, and SDIN coming from the host to the TAS5806.
We have SCLK, LRCLK, and SDOUT going to an AEC microphone array chip. (XMOS XVF3510).
Since SCLK and LRCLK are not passed through the TAS5806, we assume that SDOUT…
Part Number: TAS5806MD
Hello, while evaluating my design, I experienced that up to 18V it is okay to drive the PMT-37N28AL01-04 speaker with ferrite bead output filters. Though I am not able to drive the IC with 24V, because it would then develope too…
Part Number: TAS5806MD We are not using the Headphone amplifier function, can the HP input, output and HPVDD pins be left floating? Also, the charge pump CPP and CPN pins can be left floating?
Thanks
Part Number: TAS5806MD We are not using the Headphone amplifier function, can the HP input, output and HPVDD pins be left floating? Also, the charge pump CPP and CPN pins can be left floating?
Thanks