Part Number: TAS5825M I need to set up the TAS5825M to be able to easily change sample rates from 44.1kHz to 192kHz as described in the data sheet:
I don't need any DSP processing and am using the default rom mode 1. I have tried everything I can…
Part Number: TAS5825M Hi there,
We have an amplifier design using four TAS5825m chips and fed by a TDM8 signal.
The board is up and stable and we have no audio performance issues.
The application requires "bit correct" alignement of the output signals…
Part Number: TAS5825M Other Parts Discussed in Thread: TAS5766M , PP-SALB2-EVM , TAS2563 Do I need to characterize my speaker with a learning board for use with the TAS5825M? A few years ago I did a design with a TAS5766M and needed to characterize with…
Part Number: TAS5825M Other Parts Discussed in Thread: TAS5805 Hi. I'm Chanjong-Lee of LG electronics. We are currently using the TAS5805 and its associated SW driver(Firmware/register setting), but we intend to replace it with the TAS5825M device.
…
Part Number: TAS5825M I have a custom board that has a TAS5825M. When the board is powered at 8V it works forever without an issue. When the board is powered at 15V it works for a few minutes and then fails silently without errors. (all error registers…
Part Number: TAS5825M Hi TI
We RF team suggests adding RF De-sense R/C to the TAS5825M circuit each OUTPUT path, this is ok?
(R520,R521,R522,R523,C520,C521,C522,C523)
What should we pay attention to?
Thanks!
Part Number: TAS5825M Tool/software: Hi Lady or Gentlman:
I want to design select a adapter to power for TAS5825M. The maxmim power of speaker is 10W which drived by TAS5825M.
I am kindly look forward to help form TI and let me know how to select…
Part Number: TAS5825M Other Parts Discussed in Thread: TAS2563 , TAS2573 , TAS2781 We have encountered a speaker noise issue in our current product. When an HDMI audio source is connected from a notebook and a 200 Hz sine wave is played as background…
Part Number: TAS5825M Hi,
Could you please share the Non Integrated Device - Bin File Generator v1.4.2 ?
We are using a dual TAS5825M architecture, but currently, only the first speaker has sound—the second one does not output any audio.
Driver…
Part Number: TAS5825M Hello, I'm currently working on an amplifier board using the TAS5825M with PBTL mode and have found that immediately after the TAS5825M starts up, it throws an over-temperature exception. Below are the operating steps and observations…