Part Number: TAS5825P Hello,
We are planning to use the TAS5825P/M IC for a smart speaker. The design has one speaker permanently connected to one channel of the amplifier. The other channel may or may not have a speaker attached according to customer…
Part Number: TAS5825P Hi,
May I know how should I set the Level Meter Input Mux (Book 0x8C, Page 0x0B, Sub Address 0x34) in order to get output signal level from Level Meter Left/Right Output instead of getting input signal level?
I cannot get any related…
Part Number: TAS2781 Other Parts Discussed in Thread: TAS5825P , Hi:)
-
Just wanted to make sure if it is possible to have both the Hybrid-Pro from the TAS2781 and TAS5825P connected to each other like shown here:
In this application 2x TAS2781 and a TAS5825P…
Part Number: TAS5825P Hi, Team
Our customer feedback that our TAS5825P have a HPF(high pass filter) in our device. (1Hz to 20Hz)
They find that their test result shows: our device have attenuation between 1Hz to 20Hz.
Customer prefer check with TI, whether…
Part Number: TAS5825P Hi team,
Consists of a combination of L-channel...no signal and R-channel...audio signal Stereo signals are input to pin 14 (SDIN) of the TAS5825P as serial data and output from pin 23 (OUT_B+) and pin 27 (OUT_B-) as R-channel signals…
Part Number: TAS5825P
Hi:)
-
According to the "TAS5825P Hybrid-Pro User Guidance", when there are several TAS5825P ICs with the Hybrid-Pro feature enabled the Hybrid-Pro outputs should be set to 'Open-Drain' and connected together, along with…
Part Number: TAS5825P Hi,
We have finished TAS5825P tuning.
May I know any way to dump TAS5825P setting to any format, that we can easy let MCU set to TAS5825P when system boot up?
Thanks!
Jeff
Part Number: TAS5825P Hi team,
For the TAS58xx AMP IC, what is the minimum speed of I2C that it can support? the D/S says maximum 100kHz for the slow mode.
My customer wants to use 70kHz speed for the I2C. Can you help if this could work?
Thank you…
Part Number: TAS5825P Other Parts Discussed in Thread: TAS5825M ,
Hi:)
I am currently working on a design that uses 2x TAS5825P + 2x TAS5825M and have now come to the point where selection of a suitable Boost-Converter is required.
However I did not…