Part Number: TAS5828M Hi!
In my design using the TAS5828M for driving speakers with 8 or 4 Ohm, there occur over current errors. Here's the schematic (7A-inductors):
The output voltage span is approx 20 V, hence I can output (0.7*20)^2/8=25W (sinus…
Part Number: TAS5828M Other Parts Discussed in Thread: TAS5825M , Hello,
I reached out to TI support and they directed me here. The following indented area is the body of the email I sent. Below that describes the testing I did after sending this support…
Part Number: TAS5828M Dears,
The custoimer designed TAS5828 PBTL mode and would like to know if it is possible to use only two output inductors.
Thanks
Part Number: TAS5828M Hello,
Is the Process Flows document for the TAS5828M available yet? I've been going off the TAS5825 process flow document, but I wanted to see if updates are available as I have not been able to find the real one. My real question…
Part Number: TAS5828M hi,
is it possible to have hybrid pro +dpeq in 1.1 configuration for the TAS5828M. If not is it a device limitation or pure path limitation?
best,
hazar
Part Number: TAS5828M Hi,
A customer is reading out the DIE-ID, but they get 0x98h instead or the 0x95 stated in the data sheet. They also get this when checking what's on the I2C bus with a logic analyzer.
Is the 0x98h correct and is there a die…
Part Number: TAS5828M Hello,
I am developing a project for a multichannel amplifier. I intend to use the Digital Class D power amplifier TAS5828M. Each TAS5828M will reproduce a different audio channel from a TDM bus.
I understand how the TDM works. It…
Part Number: TAS5828M Other Parts Discussed in Thread: TAS5754M Hi ,
We use TAS5828 for speaker design, after initial parameter speaker is normal, but when I2S single off or on, speaker have pop noise output, any solution for this case? We did not have…
Part Number: TAS5828M Hi, Team
Our customer use TAS5828 in their smart speaker project, the set the GPIO as the MUTE function.
Customer prefer to know what's the response time if they set the GPIO pin to MUTE? Do we have any delay while setting MUTE pin…