Part Number: TAS5828M Other Parts Discussed in Thread: TAS5825M Hi Team,
Ctm want to use Pure Path Console 3 to generate driver code for TAS5828M, but in EVM APP, they can only find TAS5825M. Do we have TAS5828M EVM APP?
Part Number: TAS5828M Hi, team
My customer prefer to use 5pcs TAS5828M for their audio speaker project.
In their design, they will use 3.3V for DVDD. They prefer to use one 3.3V LDO (400mA) to power the DVDD for all the 5pcs TAS5828M.
Do u know What's…
Part Number: TAS5828M Hi TI Team,
Please help check the schematic diagram and Layout of TAS5828.
AS5828M Project parameters :PVDD=24V, speaker impedance 3 ω, PBTL mode, 100W, THD < 5%.
schematic
2146.TAS5828M.pdf
Layout
TAS5828M.pcb
Part Number: TAS5828M Hi
Datasheed mentioned spread spectrum and inductor less.
is there an idea how long the output trace/cable length that can be inductor less ?
Part Number: TAS5828M Hi,
Good Day.
Customer is looking for more info about the TAS5828MDADR. He have A0 and B0 devices over here but he still see some issues in the feature he want to use, so he is wondering if its a personal problem or if he is using…
Part Number: TAS5828M Hi,
Now I have done prototype test using TAS5828MDADR, but the problem is that the sound is very low.
I'm not quite clear about the reason. Could you give me some suggestions? Is there any relevant configuration document that…
Part Number: TAS5828M
Hi team,
My customer is considering two TAS5828M for their BT speaker. One for Tweeter and One for Woofer.
They will use Class-H control. And as far as I know, Class-H senses input signal and generate feedback signal to the external…
Hi Jesse,
I have reconfigured the PPC3 file for Base/Pro Hybrid 1.0 96k and enabled the Hybrid-Pro feature and set it to GPIO1 using the SRT portion of the tool. I still hear clicking from my boost power stage which can only be eliminated if the connection…
Part Number: TAS5828M Other Parts Discussed in Thread: TAS5825M We are currently using the TAS5825m, but as disponibility is indicated as 2 years away, we thought the 5828m would be a good alternative- ALAS, upon sourcing the evaluation board and installing…