Part Number: TAS6422E-Q1 Hi team,
I'm a bit confused by the dialogue in the question related to this thread. It seems that the heat sink can be electrically isolated from the heatsink (no current flow) but must still have a nearby connection to ground…
Part Number: TAS6422E-Q1 Other Parts Discussed in Thread: TAS6422-Q1 Hi Team,
The customer applied TAS6422E-Q1 to VESS.
Spec : 150 W, 10% THD Into 2 Ω at 25V PBTL
Customer checked the operation until input, but TAS6422-Q1 doesn't output.
MCLK…
Part Number: TAS6422-Q1 Other Parts Discussed in Thread: TAS6424 Hi,
I understand that TAS6422 is digital input 2-channel Class-D amp, not 4-channel Class-D amp. Therefore, it has many reserved bits in the registers for TAS6422. Then, I have a qestion. …
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424E
Hi MPA BUs,
This is Koki Tsushima. Thank you for your continuous support.
I want to ask you that does TAS6424E, TAS6424M or TAS6422 remember register setting after goes into standby…
Part Number: PCM6020-Q1 Other Parts Discussed in Thread: TAS6422-Q1 Hi, Support Team
our software team have a question:
if ADC(PCM6020-Q1) can read voltage vaule.
how to mapping digital signal related voltage value?
function block:
if any suggestion…
Part Number: TAS6422E-Q1 Hi,
I am developing A2B product using TAS6422E-Q1.
When I set the setting to 48 K H z, there is no sound, and the sound is output at 44.1KHz.
Please see the settings below and let me know what settings I am making mistakes.
The…
Part Number: TAS6422E-Q1 Hi Team,
My customer wants to find a similar chip to replace TAS6422E-Q1. They want to find a consumer chip not a Q1 chip. PBTL need support 150W. Do we have similar chip to recommend?
Best Regard
Gust
Part Number: TAS6422-Q1 Other Parts Discussed in Thread: TAS6424 I used a dsp to control and transmit audio to tas6422 .but the warn pin was pulled lower .so I want to write data control to the register through i2c but tas6422 did not respond. The response…
Part Number: TAS6422-Q1 Hi, We are using TAS6422-Q1 IC. We are using DC load diagnostics to detect the faults. During run time if the channel state is PLAY, and if short to GND and short to battery faults occurs then the Power IC will mute itself and detect…