Part Number: TAS6422E-Q1 Hello,
is it possible to input 2 separate channels, independently change their volume (registers 0x05 and 0x06) and then output mixed signal in PBTL mono mode?
-- regards Przemysław
Part Number: TAS6422-Q1 Hello everyone
I recently encountered a problem
I output the i2c signal
tas6422 cannot output signal
The value of the 0x0f register is 0x55
This shows that ch1 and ch2 are in Hi-Z state
By judging other registers, the abnormal…
Part Number: TAS6421-Q1 Other Parts Discussed in Thread: TAS6422-Q1 , We are using the TAS6422-Q1 Class-D Audio Amplifier and conducting tests related to it. We are encountering an issue and would like your assistance in resolving it. I will briefly summarize…
Part Number: TAS6422-Q1 Let me confirm the waveform of output.
Do OUT4P and OUT4M output the same waveform in PBTL mode?
and aslo, Do OUT4P and OUT4M output the reversed waveform each other in BTL mode?
Thanks!
Reversed phase
Part Number: TAS6422-Q1 Other Parts Discussed in Thread: TAS6424M-Q1 Hi
I would like to know more about TAS6422-Q1's more detailed Power On sequence.
The TAS6424M-Q1 series of products in the same series is illustrated in the following figure by sequence…
Hello Muthukumar, You need to find a Codec or DAC to drive the analog input for the TPA3112, there are no registers to configure. If you want a digital input device you can look into the https://www.ti.com/product/TAS6422E-Q1 . You can generate an i2c configuration…
Part Number: TAS6422-Q1 Hi Team, I would like to get some help for the situation of our customer below: The customer used TAS6422-Q1 in their end product powered by 14.4V (battery voltage) with two 2 Ohm loudspeakers.
The problem was, on the full volume the…
Part Number: TAS6422-Q1 Hi team,
A customer asks if TAS6422-Q1 can support I2C infertace with only VDD supply, without PVDD / VBAT.
Can you answer it?
Thanks,
Sam Lee
Part Number: TAS6422-Q1 The device doesn't have the feedback pin from output.
When voltage of the car battery is changed, how does the device keep the output gain?
Can you explain this for technical level?
Part Number: TAS6422-Q1 How can we connect a low frequency speaker Woofers (20 Hz up to 2,000 Hz) to channel 1 and Mid-range speakers range (500 Hz-4 kHz) to other channel?
Can we use filters (LC filter) between output pin and speaker to filter out each…