Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424ME-Q1 , Hi team,
Could you please clarify if there is a way to distinguish between the TAS6424E-Q1 and the TAS6424ME-Q1 through internal registers?
Thanks
Xiaoxiang
Part Number: TAS6424E-Q1 Hi team,
The datasheet indicates that the AC diagnostic time for the TAS6424E-Q1 is 520ms. If only two channels are tested, would the time be reduced to 260ms?
Thanks
Xiaoxiang
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424 , TAS6424E Hi, Team
there will be technical questions from my customer, Kyungshin.
Please support this. Thanks.
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424M-Q1 , Hello,
In order to do drop-in replacement from TAS6424M-Q1 to TAS6424E-Q1, our customer has a question about specification differecnes betwenn TAS6424E-Q1 vs TAS6424M-Q1.
while…
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424 , TAS6424E Hi team,
My customer has reported the following issue and I'd like to seek your technical input:
During electrical performance testing, with the unit powered off (GND…
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6422E-Q1 Hi team,
We found some STBY Current parameter issure from datasheet.
The customer found that the STBY current of the TAS6424E-Q1 is even lower than that of the TAS6422E-Q1. Why…
Part Number: TAS6424-Q1 Other Parts Discussed in Thread: TAS6424 , TAS6424MS Hi Team,
Iam trying to integrate the TAS6424 audio codec. The sound card is also registered. Iam using the tas6424.c driver from the kernel. Whenever I try to play, the log…
Part Number: TAS67524-Q1 Other Parts Discussed in Thread: TAS6424E-Q1 , TAS6424E Hello, Team,
We are considering whether to use the TAS67524-Q1 or the TAS6424E-Q1 for our new product development. We have obtained both EVMs and are currently conducting…
Part Number: TAS6424E-Q1 Hi TI Team, I am currently calculating power dissipation for TAS6424E-Q1,
Requirements:
Supply voltage: 12V
Number of channels: 4
Output power: 4 x 15 W, 4 ohm
Automotive qualified
For a 4 × 15 W, 4 ohm application…
Part Number: TAS6424E-Q1 Hi team,
Customer get following test and get inquiry regarding the short to power detect method:
Preconditions: VBAT = 12.5 V, PVDD = 24.5 V, channels 1 through 4 are normally connected to 4-ohm loads. Test procedure:…