Part Number: TAS6424-Q1
Hi, Support Team
our client have three question as below:
Q1: we are currently doing an experiment. I connected a cement resistor in series between the Amplifier and the Speaker, and the volume became smaller. So when the impedance…
Hi Imed
Imed said: Is there a way to smooth out these amplitude jumps?
The Volume increase is designed with fixed dB change, it's normal you would see the waveform changing quickly when power becomes larger. For TAS6424E device, there's no way to further…
Part Number: TAS6424E-Q1 Hi expert,
The customer is wondering if there is a register similar to the Fault Pin, where a certain bit of a register can be used to monitor global faults.
I am not sure if the 7th bit of 0X21 can achieve this monitoring of…
Hi Xiang
The load diag results are not included to the normal Fault state in TAS6424 device. Clear fault won't work.
We could consider using Reset to clear it. But all of the register would be reset, you'll need to re-config the one you need to…
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424-Q1 Hi There, I am getting wrong impedance value of tweeter in TAS6424e-q1 Amplifier.
I have connected two tweeter(4 ohm, 4 ohm) parallels to two speaker(4 ohm, 4ohm) to channel1 and Chan…
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424E Hi team,
Could you please advise if all channels are enabled or 1 of 4 channel only enabled for Datasheet Figure 7-5. Output Power vs Supply Voltage?
I would like to drive TAS6424E under…
Part Number: TAS6584-Q1 Other Parts Discussed in Thread: TAS6424 Tool/software: TAS6584&TAS6424 AUDIO DELAY TIME BETWEEN TDM8 INPUT AND ANALOG AUDIO OUTPUT ARE ?ms? THANK U
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424 Hello,
for an infotainment application I am using the TAS6424 Class-D audio amplifier, as this component has internal gate drive with high frequency switching I was wondering if I need to…
Part Number: TAS6424E-Q1 Hi, I am trying to get the package drawing for TAS6424EQDKQRQ1. (DKQ) datasheet does not show the detail information about dimensions and tolerances, since we are doing thermal simulations for our application, I would like to know…