Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TAS6422E-Q1 Hi dear.
Request a review for the TAS6424L-Q1. I can't buy a 2-channel audio amp (tas6422e-q1), so first I want to use a 4-channel audio amp (tas6422e-q1) to use the 2-channel output…
Part Number: TAS6424L-Q1 Dear teams,
Could I help my customer ask whether the tdelay_clipdet (signal delay when output clipping detected) is the checking time for clipping or not? If not, then whether this delay time is the time difference between the…
Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TAS6424E-Q1 Hi, team,
Can you share TAS6424L-Q1 Thermal Information? Below is capture in datasheet.
Thanks.
Johnny
Part Number: TAS6424L-Q1
Dear Support Team
I would like to get the support to review the schematic for TAS6424LQDKQRQ1
VIN: 14V
Output : 20W power for Each Channel
TAS6424LQDKQRQ1_Sch_Review.pdf
Regards,
Bala
Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TAS6424 Hi Expert,
I have some question about TAS6424
the output noise floor when no input, the output noise floor when playing music, are they the same? If not, what's the variant? Do you have…
Part Number: TAS6424L-Q1 Hi,
I'm using below audio amplifier in my design and I'm new to audio section.
TAS6424LQDKQRQ1
Do I need to route audio output (4 channels) with 100E differential impedance? or any other guidelines?
These lines will …
Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TAS6424 Hi Expert,
Our customer uses TAS6424. The input comes from MIC and it's single-end configuration. So our customer wants to know, whether they need a diode for reverse protection to "MIC1…
Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TPA3251 Hi Team,
Designing the 4channel 20W class D amplifier with TAS6424L-Q1. Chosen the LC filter, L = 3.3uH and C = 1uF based on TI reference material SLOA242A.pdf.
Is it possible to provide…
Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TAS6424LS-Q1 Hi Expert,
Our customer uses TAS6424LS-Q1 for 4Ω speaker and they already finish the schematic design. Now they want to use 2Ω speaker but they don't want to change the schematic…