Part Number: TAS6424M-Q1 Hello, Team,
Sorry for the introductory question, but could you tell us what we need to take care when using TAS6424M-Q1 with phase 0 deg? Other than EMC performance, what will be affected? e.g., efficiency, distortion rate in…
Part Number: TAS6424M-Q1 Hello,
When TDM data is input, the device automatically selects TDM mode. Is this only the case when "SAP Control (Serial Audio-Port Control) Register (address = 0x03)" is its default setting? My customer is experiencing difficulty…
Part Number: PUREPATHCONSOLE
Tool/software:
A table with links to all the software needed for audio devices and their EVMs. Find the device(s) of interest in the table and use the links to request access to the software you need.
Product or Part …
Part Number: TAS6424M-Q1 Hi Team,
From the TAS6424M-Q1 datasheet, the absolute maximum rating of VDD is only 3.5V, is there any tolerance? In my point of view, if maximum recommended condition is 3.5V, the absolute maximum rating should be higher, right…
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424E
Hi MPA BUs,
This is Koki Tsushima. Thank you for your continuous support.
I want to ask you that does TAS6424E, TAS6424M or TAS6422 remember register setting after goes into standby…
Part Number: TAS6424M-Q1 Hello
I will ask you a question for the first time in this forum.
Please tell me the difference between the phase value of "Load at Device Output" and the phase value of "Load at Filter Output" in the AC Load Diagnostics Report…
Part Number: TAS6424M-Q1
Dear TI experts,
We are using TAS6424M-Q1 for our automotive application:
- PVDD = 13.5V
- LC filter: BTL-common mode, 3.3uH and 1uF
- Load: 2 ohm, 4 channels
- We want it to run with TDM8 32bits (or 24 bits) interface, MCLK and…
Part Number: TAS6424M-Q1 Other Parts Discussed in Thread: TAS6424MSQ1EVM Hı Team,
Can you please check and advise with following request:
"
The other issue is about the TAS6424M-Q1 4-channel speaker amplifier that we want to use in the infotainment…
Part Number: TAS6424M-Q1 I am working on a car infotainment design with Vbatt ranges from 6V to 16V.
I do not want to add a buck-boost converter to maintain a fix voltage supplying to the speaker amplifier considering the board area and power dissipation…
Part Number: TAS6424M-Q1 Hello expert, I have 3questions for AC diag. First, datasheet said AC diag time is 520m[s]. Is this mean this AC diag time is measured from datasheet 9.3.7.3.1's step1? Second, Could I change Mute pin status during AC diag? For…