Part Number: TAS6424M-Q1 Other Parts Discussed in Thread: TAS6424 Application is using TAS6424M-Q1.
The customer will use the other power line for the I2C pull-up because it need to communicate with I2C when TAS6424 is off.
The question is:
3.3V will…
Part Number: TAS6424M-Q1 Other Parts Discussed in Thread: TAS6424 Dear expert,
I see that datasheet listed the output power, this is based on sine wave before clippling, right?
4 Ω, PVDD = 14.4 V, THD+N = 1%, TC = 75°C 22W
My question is, if…
Part Number: TAS6424M-Q1
Dear expert,
We use TAS6424M-Q1 in automotive IVI application with a 24pin connector for PA output to speaker wiring. Due to the 3A current limit per pin for the connector, with 12V PVDD, 2 Ohm speaker and BTL configuration,…
Part Number: TAS6424M-Q1 Other Parts Discussed in Thread: TAS6424 Dear expert,
I have a question about GAIN settings in TAS6424. The datasheet says that "The peak output-voltage swing is also configurable in the gain control register through I2C. The four…
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424MS-Q1 , Is it possible to configure this device so that the channel-to-channel PWM output phase is zero for all four channels? (like TAS6424MS-Q1)
Part Number: TAS6424M-Q1 Other Parts Discussed in Thread: TAS6424 in document slaa701 page21, it is said that "Some amplifiers require minimum inductance on the output. This specification is important to keep the amplifier reliable during an overcurrent…
Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TAS6424-Q1 , , TAS6424M-Q1 Hi Team,
My customer has a question about thermal information for TAS6424-Q1, TAS6424L-Q1 and TAS6424M-Q1. Would you help me?
The R_theta_JC(top) is 0.3C/W in the TAS6424M…
Part Number: TAS6424L-Q1 Other Parts Discussed in Thread: TAS6424-Q1 , , TAS6424M-Q1 Hi Team,
My customer has a question about thermal consideration for TAS6424-Q1, TAS6424L-Q1 and TAS6424M-Q1. Would you help me?
"Thermal Considerations" in the datasheet…
Part Number: PCM1865-Q1 Other Parts Discussed in Thread: PCM1865 , TLV320ADC6140 , PCM1690 , PCM6340-Q1 , PCM6240-Q1 , , TAS6424MS Good afternoon, colleagues!
Help with advice, we are conducting research to determine the architecture of the future version of…