Part Number: TAS6424R-Q1 Other Parts Discussed in Thread: TAS6684-Q1 , Hello TI Support,
We need to inject some communication error between MCU and Power IC.
For example on TAS6684-Q1, we can easily simulate I2C NACK error with asserted PD pin,…
Part Number: TAS6424R-Q1 Tool/software: DC diagnostic time in the datasheet only write the type 230ms,,but no have the MAX? ms,now we end the DC diagnostic time with 600ms, Please confirm:The MAX DC diagnostic time is ?ms, and the reason of 600ms(Retry…
Part Number: TAS6424R-Q1 Tool/software: Hello experts,
Custoemer uses 2.1MHz Fsw and 4ohm load in TAS6424R-Q1.
1. Any recommendation for LC filter parameter in this setting?
2. 10uH + 2.2uF is OK to use? Do you have any concern?
Thanks,
Ken…
Part Number: TAS6424R-Q1 Tool/software:
Why Fsw center is not 384k 480k after we set the SS register as below , 0x06 ATTUAL Fsw=800k-930k-1060k) 0x16(ATTUAL Fsw=720k-830k-940k)
And the setting is OK?
SETTING
NO1 …
Part Number: TAS6424R-Q1 Other Parts Discussed in Thread: TAS6424-Q1 Tool/software: We use the TMD8 format Fs=48k,BCLK=MCLK=48K*32bit*Tdm8=12.288M,all the SERIAL AUDIO PORT time match the SPEC time include Tsf Tfs Tdh Tds Tscl Tsch EXCEPT the Rise and…
Part Number: TAS6424R-Q1 Other Parts Discussed in Thread: TAS6424EQ1EVM , TAS6424RQ1EVM Will the TAS6424EQ1EVM program the TAS6424R-Q1 device for development on an external board?
I didn't see a TAS6424R-Q1 EVM and was looking to purchase both an EVM…
Part Number: TAS6424R-Q1 Tool/software: Hi TI Experts
I would like to evaluate pi LC filter design for TAS6424R PVDD/VBAT power supply, now I hope TI help to tell me how to evaluate pi LC filter design for PVDD/VBAT?
the pi LC filter is supposed to…
Part Number: TAS6424R-Q1 Tool/software: Hi team,
In datasheet, there is only description for t_start(Max)=12ms which I2C start time after VDD POR.
Is there any I2C timing requirements after standby mode? I mean, is it OK to input I2C before standby…
Part Number: TAS6424R-Q1 Other Parts Discussed in Thread: TAS6424 Tool/software: Hi,
I need access to EVM apps. I have TAS6424 eval to work on here!
Please help!
Part Number: TAS6424R-Q1 Other Parts Discussed in Thread: TAS6424 , TAS6424E , , TAS6424E-Q1 Hello TI Team,
I just found the TAS6424R chip on your webpage as new version of the TAS6424 /TAS6422 amplifieres we use in our products, and i should evaluate…