Part Number: TAS6684-Q1 Hi,
Regarding the TAS6684-Q1, we are using this in our system to drive 2x25W speakers in a vehicle application. Adding a few questions.
In our scenario, we have connected the Amplifier PVDD as well as VBATT to the same…
Part Number: TAS6684-Q1 Other Parts Discussed in Thread: AM62P5 Hi Team,
I'm integrating TAS6684-Q1 with TI am62p5 Soc, I couldnt find a linux driver namely TAS6684 in the kernel. Please provide the compatible driver, the required firmware and configuration…
Part Number: TAS6684-Q1 Hi,
In 7.3.1.1.1 Power-Up Sequence its only have timing diagram of nPD & nSTBY in different 4ms (Figure 7-1. TAS6684-Q1 Power-Up Sequence).
Could you provide timing diagram for the case where of nPD & nSTBY have to be released…
Part Number: TAS6684-Q1 Hi TI team,
We are evaluating TAS6684-Q1 for an automotive audio amplifier application.
Could you please advise whether TI has any recommended maximum speaker cable length from TAS6684-Q1 output to the speaker?
How about…
Part Number: TAS6684-Q1 Hello Team
request you to provide the TAS6684-Q Layout file.
We are looking for full gudilines of Layout, Hence request you to provide Altium Files.
In user manual all, layers of image is not given.
Regards
Prashanth…
Hi Adarsh
Adarsh Madhusoodanan said: If I am using only two channels with 4 Ω speakers , and each channel is delivering approximately 25 W output power, with PVDD = 14.4 V , how much power would be dissipated by the amplifier?
You could check the…
Part Number: TAS6684-Q1 The TAS6684 offers a closed-loop design. But how can it implement a closed loop if neither the actual output voltage nor the actual current through the speaker is measured? Only the current through the output filter is measured…
Part Number: TAS6684-Q1 Hi TI Team, Please find the schematic of Audio Amplifier - TAS6684-Q1 for review, Kindly share your valuable feedback on the same.
The design Considerations are a 4-channel BTL amplifier using TAS6684-Q1 with the following configuration…
Part Number: TAS6684-Q1
Hi TI Experts,
We have designed a schematic using TAS6684-Q1 for Automotive IVI system project.
Please review the schematic and let us know your comments.
Key parameters/design requirements are-
BTL configuration
…