Part Number: TCA6408A Our project use TCA6408A 8 GPIO all as output to control Power chip enable, due to TCA6408A output is push-pull, GPIO no PU or PD.
We tried to remove terminal power chip, just connector left, and remove source I2C, just use Aardvark…
Part Number: TCA6408A Dear Technical Support Team,
The datasheet has been updated to RevE.
Ramping up the device VCCP before VCCI is recommended to prevent SDA from potentially being stuck LOW.
Does enabling reset remove the stuck and return to normal…
Part Number: TCA6408A Hi all!
I was using the tca6408A UQFN package in my design.
As it stands, there are no TCA6408A available in any package...
I noticed the tca6408A-Q1 (TSSOP package) - Can anyone tell me if it is a direct alternative? if not, are…
Part Number: TCA6408A-Q1 Other Parts Discussed in Thread: TCA6408A Hi Expert:
We have Automotive Car infotainment project has design in TCA6408A-Q1 IO expander for MTK SoC linux driver .
The Linux driver Kernel 5.15 version called gpio-pca953x.c and…
Part Number: TCA6408A Hello,
Our customer has a question about I2C signal line condition in TCA6408A RESET initialization process. Could you let us know whether you experienced pulling I2C line low during RESET initialization process.
Best regards,
Part Number: TCA6408A-Q1 Hi Expert,
Our customer need I2C I/O expander in camera module. They have very limit space. Do you have smaller device supporting 2CH or 4CH? Automotive chip is needed. Thanks.
BR,
Elec Cheng
Part Number: TCA6408A-Q1 Hello,
I want to ask what the power consumption of TCA6408A-Q1 is when it's configured as output?
When it's input, the power consumption is low, customer want to keep input & output function normal when SOC powered off, so…
Part Number: TCA6408A Hello,
I have question about the TCA6408A.
I am currently using it with the following setup : Vccp = Vcci = 1.8V.
On the datasheet Section 6.5, the VOH of the P-port is mentioned and for Vccp = 1.65V, the min VOH is 1.2V for IOH…
Part Number: TCA6408A Hi.
I have a question.
If I2C tVD_DAT is not followed, what happens?
I think tSU_DAT and tHD_DAT is followed, there is no problem of data error.
Or could there be any problems?
I look forward to hearing from you soon.Thank you. …
Part Number: TCA6408A Hi. I have a related question.
While the main control computer, and its I2C bus and accompanying power supply for the VCCI pin is powered down, the TCA6408A output port needs to remain high.
If \RESET pin is pull to VCCP (not pull…