Part Number: TCA6416 Tool/software: Starterware I am trying to appeal to TCA6416, but the problem is that it does not respond to ASK. I check the whole l2c bus in cycle and TCA6416 is the only thing that is not seen there. I also have TCA6416 and i have…
Part Number: TCA6416A Other Parts Discussed in Thread: TCA6416 , TCAL6416 Hi Team,
We would like to have the following startup sequence, Vcci, Vccp, Reset_high. It's noted in the DS that it is recommended Vccp should come up before Vcci, with the RESET…
Part Number: TCA6416 Other Parts Discussed in Thread: TCA9539 , , TCA4311A Hi team,
My customer is planning to design a interface board to do the data transmission between difference PCB.
The TCA6416 is needed in the interface board.
So they wants to…
Hi Zekeriya,
Can you show scope captures of the I2C bus showing the NACK bit?
Are you using the pre-existing TCA6416 on the PCB, or did you solder on the TCA6416A to replace the non-A version?
Regards,
Tyler
Part Number: IO-EXPANDER-EVM Other Parts Discussed in Thread: TCA6424 , TCA6416 , TCA9535 , TCA9534 Good evening,
On my design board , which is battery powered, I need to optimize the power consumption during sleep mode ( 40uA at 3.3V) , pull-up resistors on…
Hi H@fiz,
Unlocking the thread. Is this still an open issue? If yes, could you explain the significance of PCA9543, TCA6416, TCA6424 and CDCI6214RGET? I did not follow how these devices entered the discussion.
My assumption for CDCI6214RGET is that since…
Part Number: TCA9548A Other Parts Discussed in Thread: TCA6424 , TCA9539 , TCA6416 , TCA6408 , Hi Experts,
Our customer was wondering if there were a Linux driver that's compatible with TCA9548APWR-GP. Could only identify tca6408 ,tca6416, tca6424 & tca9539…
Part Number: J7200XSOMXEVM Other Parts Discussed in Thread: DRA821 , TCA6408 , TCA6416 , TCA6424 , TCAN1042-Q1
Customer having trouble with CAN (and USB) Interfaces on this EVM.
How to configure/enable the CAN interface on the DRA821 evaluation kit (how do…
Hi Bo,
We do not have a overlay for enabling rmii on gesi board. This has been done from enet lld but not from native linux driver.
You would have to configure the pinmux and for CPSW RMII port 8 to which the phy is connected and configure the mux from…