Part Number: TCA6416A Hi Team ,
Please review the attached schematic of I2C based GPIO Expander :
Pull-up of value 10k has been added on all signals which are to be used as input ports .
Thanks,
Manoj
Part Number: TCA6416A Hi Team,
Customer is looking for alternative of PCAL6416AHF and I am proposing the TCA6416A.
and they would like to confirm if the difference is only the thermal pad size?
please help to comment. Thanks!
Patty
Part Number: TCA6416A Other Parts Discussed in Thread: TCA6408A , , TCA9548A Hello,
I am having the same problem as "user4646208": No ACK (SDA is high on ACK clock pulse) from a TCA6416A as well as a TCA6408A device.
Both devices are connected…
Part Number: TCA6416A Other Parts Discussed in Thread: TCA6424A , Hi Expert,
I want to know something about TCA6416A and TCA6424A.
* Questions
1. As I know, this device can't support ADC. Below is our customer's question.
Can the P port support…
Part Number: TCA6416A Dear Sir/Madam,
On page 17 of the datasheet "At power on or after a reset, the I/Os are configured as inputs."
If P00 to P17 are all used as outputs and the outputs need to be in a defined state before I2C access to set…
Part Number: TCA6416A Hi team, Good day.
Please help us fill out the form attached provided by the customer. Thank you.
6431.Letter of Volatility.docx
Regards, Carlo
Part Number:
Hi Support Team, In our application (battery powered), we have multiple boards, the host μC resides on board A. on Board B, I have I/O lines for status monitoring and control and I was looking at TCA6416A. Now, if I understand correctly…
Part Number: TCA6416A Other Parts Discussed in Thread: TCA6416 We are using following parts in our design and are running the thermal simulation of the product now. Can you please help share the Maximum allowable junction temperature value (Qj) for following…
Part Number: TCA6416A Hi, team,
Could you please let me know about INT feature?
1. Is there two type of use case for INT? One is a interrupt signal when data on the port is changed (input mode?) And another is signal for the indicator which is Ack / NACK…