Part Number: TCA9406 Other Parts Discussed in Thread: PCA9306 Hi Team,
Customer is asking if TI has any I2C level shift that can support 3.1MHz clock freq?
Thanks!
Andrew
Part Number: TCA9406
Hi,
I am using TCA9406 for level translation in multiple places in design. Unfortunately due to copy-paste error one of the them is also between two independent 1V8 domains, meaning that VCCB violates 2V3 requirement. The bus seems…
Part Number: TCA9406
Hi,
I need to add a 1.8V slave to my design. After looking for an I2C level translator, TCA9406 seems to be a good candidate for the job however I'm little confuse whether it is able to upper the voltage from VCCA to VCCB or lower…
Part Number: TCA9406 Hi Team,
It is mentioned in the datasheet that VCCA must be less than or equal to VCCB (except during power-on transient time), do you have a number for the "power-on transient time"?
In my application, VCCA will always be…
Part Number: TCA9406 Other Parts Discussed in Thread: PCA9306 , Hi,
I`m searching a I2C levelshifter from 1,95V to 5V Logic. I have found that two guys but I dont see the huge difference between them. Ok one has internal pullups what is good to have.
…
Part Number: TCA9406 Other Parts Discussed in Thread: PCA9306 , , TCA9511A
Hi Champs,
My customer is looking for a bi-direction I2C buffer, the competitor is LTC4315, Could you kindly suggest a suitable device for competing? I've suggested with TCA9406…
Part Number: TCA9406 Hi Team,
My customer has a question on the TCA9406. If they manually power cycle this device, would it cause any issues with other I2C devices on the same bus?
Thanks, Mitchell
Part Number: TCA9406 Other Parts Discussed in Thread: TXS0102 , TCA9803 Hi
we use a couple of TCA9406 in our project, currently our customer highlight waveform of rising/falling edge doesn't meet expectation (it seem have spike and shoulder ), the…
Part Number: TCA9406 Hello!
Do you have a maximum operating junction temperature for this device? I do not have estimated power dissipation values for this part yet, and want to set my upper limit based on your direction.
Part Number: TCA9406 Have an existing design where a TCA9406 is used between two different 3.3V Domains supplied by Power Converters on different boards.
Therefore it's possible one voltage may be slightly higher than the other, hence potentially violating…