TI E2E support forums
Menu
Search through millions of questions and answers
User
Menu
Search through millions of questions and answers
User
E2E™ support forums
Forums
Amplifiers
Audio
Clock & timing
Data converters
DLP® products
Interface
Isolation
Logic
Microcontrollers
Motor drivers
Power management
Processors
RF & microwave
Sensors
Site support
Switches & multiplexers
Tools
Wireless connectivity
Archived forums
Archived groups
Technical articles
Analog
Automotive
DLP® technology
Embedded processing
Industrial
Power management
0
TI training
Tech days
Online training
Live events
Power Supply Design Seminar
Getting started
More
Cancel
简体中文
Search tips
Showing 116 results
View by: Thread
Post
Sort by
Relevance
Oldest to Newest
Newest to Oldest
Clemens Ladisch
2 months ago
Interface
Interface forum
RE: TCA9617A: SDAB low-level output voltage
The
TCA9509
has the current source on the A side. Without a current source, I²C buffers must use a voltage offset, which implies higher output voltages. Level shifters like the PCA9306 or TCA9406 do not buffer the signals.
Gregory Duperon
over 1 year ago
Interface
Interface forum
TCA9509: A-side current source
Resolved
Part Number:
TCA9509
Is the A-side current source always active so long as VCCA is applied
Danny Bacic
4 months ago
Interface
Interface forum
RE: TCA9800: 1.8V-3.3V level shift, 1:3 MUX, bi-directional application
Jerry, Clemens is correct! You already correctly mentioned that the reason B-sides of the TCA9617A can't face each other is due to voltage offset. For clarification, this offset exists so that the device doesn't incorrectly redrive the A side...
Mitchell Kary
over 1 year ago
Interface
Interface forum
TCA9509: Question about I2C master on B side of TCA9509
Resolved
Part Number:
TCA9509
Hi, I am using
TCA9509
as a 3.3V to 1.8V I2C translation buffer. The I2C
Mitchell Kary
over 1 year ago
Interface
Interface forum
RE: TCA9509: Logic level compatibility with slave I2C devices causing problems with ACK translation
Michael Balourdas
over 1 year ago
Interface
Interface forum
TCA9509: Can this be used as an I2C repeater if both supplies are 3.3V?
TI Thinks Resolved
Part Number:
TCA9509
Hello, Can the
TCA9509
be used as an I2C repeater if VCCA = VCCB = 3.3V? The data sheet states that both supplies can take 3.3V, so it seems like it should work as the two maximum voltages are the same: But further on it states...
BOBBY
7 months ago
Interface
Interface forum
RE: TCA9517A: Request 1.8V operation in IBIS model
bryan zheng Hi Bobby, Really appreciated for your help. Since the date is not confirmed yet, could you help to find if there is any model could substitute TCA9517A. Then I can use it to do the simulation. [Bobby] For now, can you use
TCA9509
...
Clemens Ladisch
8 months ago
Logic
Logic forum
RE: TXS0102: TXS0102
The I²C specification requires that all devices drive their outputs to at most 0.4 V (see V OL at the bottom). It requires a V IL of 1.5 V to allow for noise and voltage drop over the cable. (Note: HDMI uses 5 V, so 0.3 × 5 V = 1.5 V.) A...
BOBBY
9 months ago
Interface
Interface forum
RE: PCA9515A: tie both PCA9515 SCL0/SDA0 together is fine?
Hey Bosun, I did send Annie a reply offline on the topic but just for online readers. The
TCA9509
can operate at VccA=VccB however it is outside of the datasheet spec and we do not guarantee the electrical parameters can be met at that operating condition...
BOBBY
8 months ago
Interface
Interface forum
RE: TCA9617A: B-side to B-side adaptation stage
Hey Etienne, Sorry for the delay in response. I took a look at the powerpoint you posted but I see a problem with the TCA9617A being connected to A side of
TCA9509
. B side of the 9617 has a static voltage offset and A side of the 9509 has an offset...
<
>
Didn't find what you are looking for? Post a new question.
Ask a new question