Part Number: TCA9534A Other Parts Discussed in Thread: TCA9555 Can you change the address of the TCA9534A when its powered on by changing the state of the address pins or can this only be changed when the device is powered on. If it can not be changed…
Part Number: TCA9534A Hi Expert,
Could you help to know the different of below parts?
and if the spec request:
VCC :1.6V to 5V
channel: 8 port
Which one is nice choice?
Best Regards,
Mark
Part Number: TCA9534A Other Parts Discussed in Thread: TCA9534 , Hi~
May I know the difference between TCA9534 and TCA9534A?
Thanks and Best regards,
Tiger
Part Number: TCA9534A Hi team,
My customer wants to know when /INT is reset.
In the datasheet page.17 8.3.2 Interrupt Output (INT) section, there is a description that "Resetting the interrupt circuit is achieved when data on the port is changed to the…
Part Number: TCA9534A Team,
Customer is using this chip, we are wondering about the behavior on the port pins in terms of noise immunity/hysteresis, debounce situations, etc. The datasheet shows a VOH, and an IOL, which is a bit confusing.
Thanks!
…
Part Number: TCA9534A Other Parts Discussed in Thread: LM75B , TCA9534 , Hello,
I am having issue getting a TCA9534APWR to work on my prototype.
I ma using a PIC32 as I2C master, with library I have used with no problem for years.
On the same I2C line,…
Part Number: TCA9534A Dear all,
I would like to communication like attached file.
comunication flow.pdf
Are there somwthing wrong to communicate?
If you need some condition to check, please inform us what is not enough.
Best regards,
Part Number: TCA9534A Dear all,
I want to use this device as output and default output level as "L".
To achieve this usage, I think to set as following sequence.
>1, set register 1 to change default output value as "L"
>2, set register…
Part Number: TCA9534A Dear all,
■QUESTION
After I set the direction setting of I/O port,
if I write the same direction setting to Register 3 (Configuration Register) again during output or input control,
are there influences on the output signal or input…