Part Number: TCA9546A I looked through the datasheet, but it was not clear to me if it is specified the delay from switching the mux to a different path and when it is ready to send data.
Part Number: TCA9546A Other Parts Discussed in Thread: P82B715 hi TiTeam,
can you suggeste an equivalent Part with a input bus voltage range beond 20 V or at least 20 V not the max 7V?
Or do you may have an extended specification for the part?
Best…
Part Number: TCA9546A Dear TI members,
There are some spec questions need to confirm with you.
1. The definition of Vpass is "Switch output voltage" in the spec. This will confuse our customer that we need to reference Vpass to decide the output voltage…
Part Number: TCA9546A Other Parts Discussed in Thread: TCA9548A Dears,
Could Ti support TCA9546A example drvier code, thanks.
My customer uses it in gas meter application having this required.
Part Number: SN74LV4052A Other Parts Discussed in Thread: TCA9548A , TCA9546A , , SN74LV4051A Hi team,
do we have recommendation for below requests?
1. 4ch 2.3-5.5V I2C/SMBUS MUX
2. 8ch 2.3-5.5V I2C/SMBUS MUX
Part Number: TCA9517 Other Parts Discussed in Thread: TCA9546A , Hi Sir,
We just found if we connect TCA9517 B side to TCA9546A, the I2C can't work, as below topology.
But if we swap TCA9517 A-side to connect with TCA9546A, the I2C work well.
Could you…
Part Number: TCA9546A Hi Team,
My customer current design is let CPU to reset TCA9546A, but during the board bring up, CPU can’t to reset TCA9546A.
(Because they use CLK gen IC to supply all of system CLK, but it use I2C to configure the CLK output…
Part Number: TCA9546A Hi Folks,
Does this part act as a buffer, or just a switch. I like to know if we need to place a I2C buffer on the chain to be compliant with <400pF.
The data sheet says maximum allowed capacitive load is 400pF, just wanted to…
Part Number: TCA9546A Other Parts Discussed in Thread: PCA9546A , PCA9548A HI
my customer have questions about the signal testing and simulation on TCA9546A.
they asked me that input signal and output signal is separated or connect to together.
they need…