Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: ESD2CAN24 , CSD , CSD17483F4 , CSD87502Q2
Tool/software:
Hi Team,
My application includes a CAN interface, which requires GPIO control for enabling and disabling the 120ohm CAN termination…
Part Number: TCAN1042-Q1 Tool/software: Hi E2E,
Our customer is sorting out the design document .
They want to get TCAN1042-Q1 C&S conformance test report, please help to provide it.
Many Thanks
Part Number: TCAN1042-Q1 Tool/software: What would cause the CAN lines to both drop below the recessive level at the same time? In the picture below, it seems it occurs when the second device is powering up. Is there a temporary state of a device being…
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: ISO1042 , SN6501 Tool/software: Hi,
I'm thinking about using TCAN1042 transceiver in my project to connect two boards in between. There will no be GND connection in between these two boards,…
Part Number: TCAN1042-Q1 Hi Team,
Could you please kindly help to check for TCAN1042 terminal resistor as below R7 and R15 shows, why a 0805 package size resistor is needed here? What would be the maximum power through these resistor? Thanks a lot for…
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 , Hi,
Dose tcan1042 support hot plug? By hot plug, I mean two already powered up devices connect CANBUS with cable.
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 , Hi team,
My customer uses TCAN1042DRQ1 in their project. And they met below question, could you please help give some comments? Thank you!
For the TX dominant timeout feature…
Part Number: TCAN1042-Q1 Dear TI expert,
Our product uses TCAN1042-Q1 as the CAN transceiver, we found a problem during the test, after the 1042 is awakened, it will continue to output a low level of 2ms, which causes the receiver device to continue…
Part Number: TCAN1042-Q1 Dear TI experts,
My customer asked the location of resistors in communication line. Could you check that which one is right for case 1 and case 2?
Case1) 250Kbps communication speed.
1-1. 120ohm resistors are located in…