Part Number: TCAN1042H Hi team,
Regarding TCAN1042HGVDR, customer wants to test the electrical-related items for high-speed CAN lines. Could you please share that if you have? for example, voltage level, date rate. etc.
Nison
Part Number: TCAN1042H Other Parts Discussed in Thread: TCAN1042-Q1 Hi Team,
Do we have CAN pspice model (or other spice model) or plan to develop? Any non-isolated or isolated CAN model are OK. Thanks.
Best regards,
Yang
Part Number: TCAN1042H hi,
my account had populated TCAN1042HDR on its MP boards according to below schematic in which NC (pin5) is directly connected with 3.3v. Are there any risks for TCAN1042HDR?
Part Number: TCAN1042H-Q1 Other Parts Discussed in Thread: TCAN1042H Hi Team,
Please share the +-70V bus fault test report of TCAN1042H. My customer would like to check it. Thanks.
Regards,
Alex
Part Number: TCAN1042H tHE BUS FAULT VOLTAGE MEANS WHEN THIS VOLTAGE APPEARS ON BOTH THE LINES OF THE COMMON MODE CHOKE ,i ASSUME THIS WOULD BE RELATED TO WITHSTANDING VOLTAGE OF THE TWO LINES OF THE CHOKE AND NOT WITH RELATED TO THE ACTUAL POWER SUPPLY…
Part Number: TCAN1042H-Q1 Other Parts Discussed in Thread: TCAN1042H Hi
May customer is not sure if they need 70V fault protection or not.
may i ask in which scenario may cause +/- 70 fault protection need for the CAN transceiver ?
and how do i check my…
Part Number: TCAN1042H Other Parts Discussed in Thread: ISO7741 , ISO1044 , ISO1042 Hi Expert,
My customer just want to ask the ISO7741 can connect with our CAN FD TCAN1042 or not ?
Or we have combo solution for this application ?
Eddie
Part Number: TCAN1042H Hi Team,
My customer can easily find error frame when they increase the devices on the CAN bus.
Is there any guidance to solve this problem?
Regards,
Charles