Part Number: TCAN1042H Hi team,
I am wondered how is the 'BUS Fault Protection' voltage is defined? Is the fault voltage is defined as CANH or CANL to CAN GND? Or the fault voltage is differential voltage between CANH and CANL? If the answer is the former…
Part Number: TCAN1042H Hi Team,
Customer is consulting how to do lightning protection design. Do we have some design material to share w/ them? Thanks.
Best,
Stanley
Part Number: TCAN1042H-Q1
I see that 58V BUS voltage is sufficient in ISO 11898-2:2016(E) standard. What is the advantage of "TCAN1042HDRQ1" integrated with 70V BUS voltage?
Part Number: TCAN1042H Hi
Is there a Support CAN BUS FD and socket can solution that can be recommended? Customers need to support X86 platform and Linux driver, please help me to confirm~Thank you.
Part Number: TCAN1042H Hi team,
My customer wants to know if they can left the GND pin of TCAN1042 floated, while only CAN_H and CAN_L are linked out to the bus, as shown in the following figure,
The isolated power is powering TCAN1042 via Vcc and STB…
Part Number: TCAN1042H Hi Team,
Do we have maximum value for differential output signal rise/fall time? There is only typical value in datasheet.
Regards,
Part Number: TCAN1042H Other Parts Discussed in Thread: TCAN4550-Q1 , TCAN1144-Q1 , TCAN1044-Q1 , TCAN1042-Q1 We need CANBUS solution with SPI interface to replace competitors. Could you suggest some devices for us?
Solution1: CAN Transceiver with SPI in…
Part Number: TCAN1042H Hi Team,
Customer is asking about Driver dominant time out - Data rates down to 10 kbps spec, how is it determined? through Dominant timeout spec?
Customer would like to know detail.
Thanks!
Andrew
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: DRV8353R VCC and Gnd pins of TCAN are found short when we removed IC out of board as it was not functioning.
Is there any specific root cause for such internal short?
We are using buck converter…
Other Parts Discussed in Thread: TCAN1042H Hi there,
I am looking for CAN transceiver IC options with bus fault protection voltage higher than 75V. Do you have any recommended solution? The closest I could find is TCAN1042H, but it is only rated to 70V…