Part Number: TCAN1042H-Q1 Other Parts Discussed in Thread: TCAN1042HV-Q1 Hello Team,
One of my customer tested, short to battery (+60V) for the CAN bus line within the rating given in data sheet for TCAN1042HV-Q1
Actions and Observations:
We connected…
Part Number: TCAN1042H Other Parts Discussed in Thread: TCAN1042-Q1 Hi Team,
Do we have CAN pspice model (or other spice model) or plan to develop? Any non-isolated or isolated CAN model are OK. Thanks.
Best regards,
Yang
Hi Clemens,
a long list of part # are with 1042V top marking
Can you help also check the date code the exact part # it is ?
the device fail 70V fault protection test. customer would like to confirm if it is TCAN1042H?
non "H" version of device like TCAN1042VDR…
Part Number: TCAN1042HV-Q1 Other Parts Discussed in Thread: TCAN1042H Hi Team,
When I add 60V voltage from the CANH and CANL pins, it will burn out. What is the test protection conditions for ±70V?
Mark,
Additionally, please note that this is TCAN1042HV, not TCAN1042HV-Q1. This top marking is for a TCAN1042HVDR; see this other e2e post:
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1306722/tcan1042h-can-you-help-look-up…
Part Number: TCAN1042H-Q1 Other Parts Discussed in Thread: TCAN1042-Q1 hi Team,
customer looking for a smaller package size of TCAN1042
1. the VSON package seems only available for TCAN1042 - Q1 device? is there non-Q device that also in VSON package…
Ahmed,
The only CAN devices in our portfolio that are rated this high are TCAN1042H-Q1 and TCAN1043H-Q1. I would recommend the TCAN1043H-Q1 in this case to give a bit more system configurability.
Regards,
Eric Hackett
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1042HG , TCAN1042H , TCAN1042HV , TCAN1042HGV , TCAN1044A-Q1 Hi expert,
Do you any industrial P2P replacement of TCAN1042-Q1? Thanks.
Regards,
Jared.