Hi Jack,
The
Jack said: HS CAN may follows the CAN Protocol C and ISO11898-2
On ISO11898-2
The ISO 11898-2:2016 is a physical layer standard whereas 11898-1:2015 is the data link layer.
CAN transceiver on the DRA821 EVM (TCAN1042) also supports…
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1042HG , TCAN1042H , TCAN1042HV , TCAN1042HGV , TCAN1044A-Q1 Hi expert,
Do you any industrial P2P replacement of TCAN1042-Q1? Thanks.
Regards,
Jared.
Hello,
- Yes, of course I am attaching the schematic of the power module.
- Yes, it is correct the design is separated by a connector. When the integrated LP87702-Q1 fails, it no longer recovers. I have unsoldered the connector and I have measured…
Part Number: IWR6843 Other Parts Discussed in Thread: IWR1843 , , AWR1843 , IWR1843BOOST Dear team,
I have some questions about the mmWave Radar IWR1843 and IWR6843.
1. Since I am working on enabling beamforming for the radar, I am looking for a way…
Hardware modification:
AM243x EVM + OSPI PSAM schematics:
PROC101E1_OSPI_SCH_AM243x.pdf
Note: Above schematic can be used as a reference. Currently this board is not sold in TI.com
To enable OSPI PSRAM a high-speed switch was added to the board…
Part Number: AM2431 Other Parts Discussed in Thread: AM2434 HI Team,
We are facing an issue while trying to connect to our custom AM2431 board through JTAG (using CCS).
The error shown is:
Error: SC_ERR_PATH_BROKEN (-233)
The JTAG IR and DR scan…
Part Number: CDCLVC1310 Other Parts Discussed in Thread: AM6421 , Hello, We are using CDCLVC1310 clock buffer in one of our designs which is based on AM6421 processor. While refering to EVM schematic "PROC101C(004)_SCH", we found some hardware circuit…
Part Number: TCAN1042-Q1 As the title requests, what is the maximum input rise/fall time for the TXD input? I would expect this differs between the "V" and "not-V" variants, given the TTL vs CMOS logic levels.