Part Number: TCAN1044AEV-Q1
Tool/software:
Hello Team,
I am using TCAN1044A as my can transceiver, is it recommended to have a choke on the can high and can low line ? could you also please explain the difference in single and split line termination…
Part Number: TCAN1044AEV-Q1 Tool/software: Hi,
I'm currently working on a design that uses the TCAN1044 IC for an EV application. In the datasheet it's given that the absolute maximum rating of the IC is -58V to +58V, though for a limited amount of…
Part Number: TCAN1044AEV-Q1 Tool/software: When testing with VCC = 5V, VIO = 3.3V, I have observed the RXD pin erranously being pulled to 5V. I have 10k pullups to 3V3 on each line. Is it possible this is a hardware fault with the IC?
Part Number: TCAN1044AEV-Q1 I'm trying to use an FDCAN interrupt to wake up the STM from standby state. I have features that allow me to get into and out of sleep states. Exist any choices for utilizing standby mode? I'd appreciate any guidance on this…
Part Number: TCAN1044AEV-Q1 Hi team,
When using split termination with TCAN1044AEV-Q1, how can we calculated CSPLIT value?
SLLA270 mentions CSPLIT=4.7nF with 1.1Mbps. How can we determine CSPLIT when the data rate is 4Mbps with RL=120ohm?
Best…
Shubham,
Shubham Jagtap said: There is 2 Node - One is our product having a TCAN1044AEV-Q1 and other Product - We don't have a access but we will check for their transceiver.
Ok, I see, thanks for the note. If the EN line is also visible to this other…
Part Number: TCAN1044AEV-Q1 Hi Team,
Good day!
The customer apply a request.
They received the request of the data of EMC (Emission) based on IEC 61967-4 or IEC62228-3 (150 ohm method) from automotive customer. TCAN1044AVDRQ1 supports the test and…
Hi Eric-san, Thank you for making the plan to revise the datasheet.
The following excel shows the list of document number which has the typo. I'm glad to help you identify the devices which should be revised.
Typo_TCAN1044xxx.xlsx
Best Regards…