Part Number: TCAN1057A-Q1 Hi Team,
Then we found that whenever CAN_TX has data, the waveform of CAN+/CAN- will suddenly "shift" as a whole and then slowly return to normal So when there is a lot of data, it seems that CAN+/CAN- signals suddenly…
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1057A-Q1 , TCAN1044A-Q1 , TCAN1057-Q1 , Hi Expert,
Customer would like to do the compatible design between TCAN1042 and TCAN1057. Would like to check with you if PIN5 NC of TCAN1042 can connect…
Toshi,
Please see the attached spreadsheet. Also, the ESD2CAN24 is not our device, that belongs to the INT-PD team. We filled in as much as we knew for that device.
Self Risk Assessment Check List_TRX_CAN_LIN.xlsx
Regards,
Eric Hackett
Part Number: TCAN1057AV-Q1 Hi, this is Sun Ho Park in LG electronics.
I have a question about a description of red box comment in TCAN1057 datasheet.
Does this mean,
When TCAN1057 receives open-drain output from AP or MCU , external pull-up resistor…
Part Number: SN65HVD232 Other Parts Discussed in Thread: TCAN1057-Q1 Hi Team
Customer legacy project used SN65HVD232 with 5V power rails. They found this device is not for 5V power rail until recently.
But the circuit work well in the past and no failure…
Part Number: TCAN1057A-Q1 Other Parts Discussed in Thread: SN65HVD251 Hi Team,
I promoted TCAN1057 to customer for CAN communication, I see there are two spec in datasheet: 8mA max ratings and 2mA continued recommended. Could you please help me further…
Part Number: TCAN1057AEV-Q1 Other Parts Discussed in Thread: TCAN1057A-Q1 , TCAN1057AV-Q1 , TCAN1051 I am given part number TCAN1057GVDRQ1 as part of the BOM for my project. However, I am not able to find this part on the TI web site or on any semiconductor…
Part Number: TCAN1057A-Q1 Other Parts Discussed in Thread: TCAN1051-Q1 Besides, I would lilke to know
1.Why TCAN1057A-Q1 is Non-RoHS part, does TI have TCAN1057 which is compiant with RoHS?
2.Why TCAN1051-Q1 is RoHS compliant? What is the difference? …
Part Number: TCAN1057A-Q1 Hi team,
My customer will use TCAN1057 for 1Mbps UART communication BUS. This BUS has 2 follower nodes and the each harness length is around 6m on star connection.
My customer want out advice what EMC caring should be done. Could…