Part Number: TCAN1145-Q1 Hello team,
I have a couple of questions regarding the device state.
1) In case of switching to sleep mode with VSUP, VIO and VCC then the VIO and VCC are removed after a period of time, will it be stayed in Sleep mode? (If a trigger…
Part Number: TCAN1145-Q1
1. Can TCAN1145-Q1 realize the STB( short to battery) and STG(short to ground) diagnostic? If do, how to realize these two features?
2. When using TCAN1045, when there are always error frames on the CAN BUS, TCAN1045 cannot sleep…
Part Number: TCAN1145-Q1 Hi team,
1.What is the internal structure of the TCAN1145-Q1‘s WAKE pin(Pin9)? Is there a pull-up or pull-down resistance? If so, what is the resistance value?
2. Could you please help review the schematic and give some…
Part Number: TCAN1145-Q1 HI All:
TCAN1145 as the non-terminal node of CAN bus .There are a total of 10 nodes on the bus,the length of the harness is 1.3m,What should TCAN1145's terminal resistor be.
Part Number: TCAN1145-Q1 We want to use TCAN1145 to replace TJA1145, now the package is the same, but I find the datasheet chapter10.6 Register map is not the same with the TJA1145,
TCAN1145 replace TJA 1145,Whether the software needs to be modified. Is…
Part Number: TCAN1145-Q1 Other Parts Discussed in Thread: TCAN1042H TCAN1145-Q1, in normal operation, CANH and CANL will be burned out if short-circuited to 32V.
Part Number: TCAN1145-Q1 For TCAN1145DMTRQ1, we need to understand if this part, which has Cu bond wires, is AECQ-006 qualified. The Qualification report that I downloaded seems to indicate that it is not qualified to the AECQ-006 standard, but I need…
Part Number: TCAN1145-Q1 Hi team,
The customer proposed the following solution, please help to see if it is feasible?
I feel it is similar to this description.
Part Number: TCAN1145-Q1 Hi team,
To initialize the transceiver chip, what registers need to be set? Do I need to distinguish the order in which these registers are set? Look forward to your reply, Thanks. Regards, Amber