Part Number: TCAN1463-Q1 Other Parts Discussed in Thread: TCAN1043A-Q1 Hi, team,
We are promoting TCAN1463-Q1 in customer, some questions below may need your support to close.
1. If changing from TCAN1043A-Q1 to TCAN1463-Q1, do we need to consider the…
Part Number: TCAN1463-Q1 Hi, Support Team
We want to replace TJA1463, but some Electrical Characteristics didn't see in datasheet.
Please help to check.
1. Standby mode current w/o V IO (max) ?
2. Standby mode current w/ V IO (max) ?
3. WUP Filter time…
Part Number: TCAN1463-Q1 Hi TI Expert,
I notice the TCAN1463-Q1 has a parameter called RID(dom).
For the ISO 11898-2, we have to maintain the impedance within 50~60 ohm with 1.5V CANH-CANL.
But RID(dom) is only 40 ohm so I'm wondering whether it will…
Part Number: TCAN1463-Q1 Hi team,
I have some question regarding TCAN1463-Q1 Pin usage.
Could you give comments for below?
1. INH
Is it used for toggle enable (power by DCDC) when device wakes up from sleep by CAN input?
2. Wake
2-1. It seems that…
Part Number: TCAN1463-Q1 Hi,
Customer had a question about designing layout of TCAN1463DMTRQ1.
They have difficulty applying thermal vias due to layout in bottom layer, and considering not using them(: 0.2pi, 6EA in layout pic below).
Is there any issue…
Part Number: TCAN1463-Q1 Other Parts Discussed in Thread: AWR6843AOP , Dear Team
What configuration is need to support 8Mbps by TC1463-Q?
MCU : AWR6843AOP
CAN TRx : TCAN1463-Q1
Test Application : ti/ mmwave_sdk_03_05_00_04/package/ti/drivers/canfd/test…
Part Number: TCAN1044AV-Q1 Other Parts Discussed in Thread: TCAN1463-Q1 , TCAN1043A-Q1 , Tool/software: Hi CAN Team,
My customer is using TCAN1044AV-A1, TCAN1043A-Q1 and TCAN1463-Q1, and found frame error when one of CAN BUS was opened.
OEM is asking to…
Part Number: TCAN1463-Q1 Dear Sir or Madam,
are there already electrical characteristics for this new CAN transceiver? Especially the power consumption for the different voltage levels Vsup, Vio and Wake would help a lot to implement the IC in a new…
Part Number: TCAN1463-Q1 Other Parts Discussed in Thread: TCAN1043A-Q1 Hi, My customer has 2 questions for TCAN1463-Q1.
1. If any failure is occurred on CAN BUS, can the device detect the failure? Where, the assumed failures are 1-1 Either CANH or CANL…