Part Number: TCAN4551-Q1 Other Parts Discussed in Thread: TCAN4550 , TCAN4550-Q1 , MSP430FR6989 Hi,
We are looking for driver code on the SPI side of the chip. You can assume the SPI interface of the TI micro-controller. If the said code demonstrates CAN…
Part Number: TCAN4551-Q1 Other Parts Discussed in Thread: TCAN4550-Q1
I have a question to ask. The meaning of this sentence is: If we use an IO voltage of 1.8V, we cannot use crystals, right?
Why should an external clock be used instead of a crystal…
Part Number: TCAN4551-Q1 Hello team,
Is nINT pin the default pin for interrupt signal?
What are the use case for GPIO1 and GPIO2? Are they used for some specific interrupts?
Best Regards,
Kei Kuwahara
Part Number: TCAN4551-Q1 Other Parts Discussed in Thread: TCAN4550-Q1
Hello team,
Will the setting of SWE_DIS reset, after power off, and powered on again?
Best Regards,
Kei Kuwahara
Part Number: TCAN4551-Q1 Hello team,
What are the types of wake up events does TCAN4551-Q1 support? Are they just LWU and WUP?
Also, could you list the power state (Normal/Sleep/Standby) each wake up event support?
Best Regards,
Kei Kuwahara
Part Number: TCAN4551-Q1 Hello team,
My customer has 4 questions on the nWKRQ pin.
1. Is there any timing chart when 16'h0800[8] = 1? On the datasheet, it seems that the timing chart represents when 16'h0800[8] = 0 as the nWKRQ is related to INH state…
Part Number: TCAN4551-Q1 Hello Team,
My customer has question regarding VIO of this device.
What will happen if VIO is off during normal or standby mode? There is no explanation of VIO on datasheet Fig 22. device state diagram.
I believe it is okay for…
Part Number: TCAN4551-Q1 Hello team,
What is the maximum voltage of FLTR pin? On the datasheet, it only describes TYP value.
My customer is concerned that he can only get 0.33uF cap with 6.3V max voltage tolerance.
Best Regards,
Kei Kuwhara
Part Number: TCAN4551-Q1 Hello,
Good day!
I'm using TCAN4551 in my design. Will it support only Mode 0 (CPOL=0, CPH=0), or other configurations were also possible?
Thanks,
Swathi