Part Number: 66AK2L06 Dear all,
I am facing an issue with loading the CCS compiled executable using mpmcl load command.
But, using CCS it is loading and executing well.
Observing the following error on loading.
root@k2hk-evm:~# mpmcl load dsp4 exe.out…
Hello TI Team,
we would like to test our DDR3 - ECC enabled design by injecting single and double errors. I went over documentation, and unfortunately I havent found means to inject errors.
Could you please help with this? How can we test ECC i.e. inject…
Hi,
The Q-PEND Queue mapping to the interrupt on ARM of TCI6638K2K, is given below.
/* System Interrupt Mapping for INTC_SET2 Queues */ const int32_t intcSet2Mapping [] = { 40, /* Queue 658 */ 41, /* Queue 659 */ 42, /* Queue 660 */ 43, /* Queue 661 …
Hi all,
On loading the ti/mcsdk_bios_3_01_04_07/tools/program_evm/binaries/evmk2h/nor.bin file, following error has occurred.
SEVERE: C66xx_0: Trouble Reading Memory Block at 0x80000000 on Page 0 of Length 0x4: (Error -1202 @ 0x80000000) Device core is…
Hi Team,
We are using TCI6638K2K. We are connecting three devices using the hyper links between each other. I have following question in that regard-
1.Hyperlink Serdes Architecture Document for the Keystone 2 devices is not available . Is there any…
Hi Team,
We are using TCI6638K2K. We are connecting three devices using the hyper links between each other. I have following question in that regard-
1.Hyperlink Serdes Architecture Document for the Keystone 2 devices is not available . Is there any…
Hi TI Team,
We use TI Keystone-II (TCI6638K2K) SOC in our board, we are trying to bring-up PCI interface in this chip, it is concluded that the PCI register space is not accessible, it throws an exception with Bus Error in Linux kernel, whereas in U-boot…
Part Number: TCIEVMK2X Other Parts Discussed in Thread: CDCM6208 Hi,
we are observing ASCII extended character 193 instead of 67 for CCCC in Uart mode in a K2K board.
We observed the clock to be ok. we are able to see the Sys_clock input to processor is…
Part Number: PROCESSOR-SDK-K2H Hello,
We are using TMS320TCI6638 in one of our enodeB design.
We are not getting CCCCCCC in the console in th UART mode.
but we are able to observe the pulses at the SoC UART0 TX output.
Kindly advice what cloud be the problem…