Part Number: TDA2EG-17 Other Parts Discussed in Thread: TDA2E , TPS65919-Q1 , LP8733 Hi team,
My customer is using the TDA2E platform, the solution is PMIC(TPS65919)+SOC: TDA2EGBHQCBDQ1, they find two power sequence and don't know how to select, please…
Part Number: TDA2EG-17 Other Parts Discussed in Thread: TDA2 Hi,
Customer they met one urgent issue, they choose a GD flash that only support the mode, from which that input data is latched on the rising edge of SCLK and data shifts out on the falling…
Part Number: TDA2EG-17
Dear all,
I want to make OSD on panel
I was only looking at "GrpxSrc -> Display_Grpx"
But It does not seem to support png display on panel
I like to make the picture (ex./home/Image.png) like " null_src_dec_display …
Part Number: TDA2EG-17 Hi, expert:
One of my customers is evaluating TDA2EG-17 for CMS applications.
In this project, FOTA (firmware update) function is planed via ethernet.
So, customer is checking with us whether the UDP broadcast is supported…
Part Number: TDA2EG-17 Hello,
终端打印如下:
DRA722-GP ES2.1
running dra7-ipu2-fw.lzop success...
running dra7-dsp1-fw.lzop success...
Trying to boot from MMC1
*** Warning - bad CRC, using default environment
spl: falcon_args_file not set in environment…
Part Number: TDA2EG-17 Other Parts Discussed in Thread: SYSBIOS
Hi,
SDK: ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03
4 camera--->ds90ub964---mipi csi--->tda2e-17.
Do the four cameras have to be synchronized? Can the camera be without…
Part Number: TDA2EG-17 Other Parts Discussed in Thread: LP8732-Q1 , LP8733-Q1 Dear Team,
Our customer have some question as below,
In theory, it should start at the same time, but there is a 1.5ms start difference, according to (LP8733-Q1 and LP8732…